Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General QSPI boot / update
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 373 subscribers
  • Views 2938 views
  • Users 0 members are here
Related

QSPI boot / update

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I would like to confirm few things.

I am planning a design with Zynq + QSPI+eMMC and have few questions related to that.

 

1) If I choose to use qsPI as boot; the QSPI can be updated (=write/read) with Linux on the fly easily using same SPI pins that they are originally assigned ?

Meaning that these QSPI pins can be accessed by Linux also in user mode ? The qSPI are NOT dedicated to the boot only ?

2) If using QSPI as a boot, eMMC can be used as a storage memory ?

 

3) If using eMMC as a boot source, the same eMMC can be used as a storage memory at the same time ?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Partly answeroing to myself..

    Should this be done via U-boot in two stages?

     

    First load u-boot to QSPI  (=fsbl+u-boot) and boot from and there:

    1)make eMMC format and place eMMC boot parts to there (bitstream+uboot+OS)

    2) and then update the QSPI with FSBL with emmc_support

     

    Or how ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Partly answeroing to myself..

    Should this be done via U-boot in two stages?

     

    First load u-boot to QSPI  (=fsbl+u-boot) and boot from and there:

    1)make eMMC format and place eMMC boot parts to there (bitstream+uboot+OS)

    2) and then update the QSPI with FSBL with emmc_support

     

    Or how ?