Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General timestamping inputs to the nanosecond
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 530 views
  • Users 0 members are here
Related

timestamping inputs to the nanosecond

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I don't know much about FPGAs, but from the information I could gather they can be a great answer to my quest; I think especially the MicroZed could be the magic I'm looking for to implement what I need. Could some of you tell me if it's doable ?

Here are my needs: I have a few inputs (about half a dozen) which are square 1Hz signals, more or less stable. For each signal I need to precisely timestamp its rising edge with respect to a very precise master clock (also 1Hz), down to a nanosecond measurement.

Is it possible to do that with a Zynq ?
Does it leave some "free space" on the FPGA to implement other functions ?

Thanks,
        Xav

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago
    Hi there,   The MicroZed product line has Artix fabric, which is more power efficient and lower speed than his faster bigger brother using Kintex fabric. Using Vivado and the Zynq 7020 version as a test, I am able to see that the Clocking Wizard only allows you to configure the internal clocks to 800MHz MAX. I then changed to a 7030 (the fastest PicoZed), which also demonstrated a clock limit of 800MHz. This does not go higher until you start getting into higher speed grades (933Mhz and 1066Mhz).   I would suggest you look at using the FMC Carrier card  http://microzed.org/product/microzed-fmc-carrier with a custom FMC card similar to this one:  http://www.sevensols.com/index.php?seccion=1400&subseccion=1439   It seems that card will do exactly what you need!   To answer your questions, without doing something with external hardware, I do not think that you are going to get to a nanosecond of accuracy with the Zynq family due to the speed capability of the input pins as well as clock frequency specifications. If you use the above listed card, I feel that there will be plenty of room in the Zynq to do many things and implement many functions. Especially if you look at leveraging the built in hardware accelerators which do not take up any logic except what you need to link those accelerators to any logic that you intend to use. If you use the function directly, there is 0 cost to the fabric of the Zynq!  --Dan
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to drozwood90

    Hi Dan,

    thanks for your answer. I have seen some papers where they do time measurement with greater precision than the FPGA's clock by using "carry chains", e.g.: http://pwt.et.put.poznan.pl/PWT_2012/PWT%202012_2242.pdf
    Is that possible with the Zynq ?

            Xav

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to drozwood90

    Hi Dan,

    thanks for your answer. I have seen some papers where they do time measurement with greater precision than the FPGA's clock by using "carry chains", e.g.: http://pwt.et.put.poznan.pl/PWT_2012/PWT%202012_2242.pdf
    Is that possible with the Zynq ?

            Xav