Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Use of Zedboard within commercial product
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 372 subscribers
  • Views 427 views
  • Users 0 members are here
Related

Use of Zedboard within commercial product

e14 Contributor
e14 Contributor over 13 years ago

I'm wondering if there are licensing issues with using the the Zedboard within a commercial product, or in combination with a commercial product such as a custom FMC mezzanine card?

This would save smaller companies a lot of expense in creating their own custom silicon around the Zynq FPGA which would essentially perform the same tasks as the Zedboard.

I know that it is not possible with Xilinx Development boards as per this post;
http://forums.xilinx.com/t5/Xilinx-Boards-and-Kits/Does-anyone-use-Xilinx-evaluation-board-in-production-system/td-p/144876

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    In the Xilinx forum thread that you reference, the Avnet response was

     

    If there is a compatible Avnet board with FMC that will work for you, then Avnet Engineering Services will build them for your production.
       ...

     

    You can also negotiate some customization if there are features you want removed to save cost or changes that you want on your build (different speed grade FPGA, for example).

     

    If you are interested in this, please contact James.Jaksich@avnet.com

     

    That would apply here as well.

     

    You could also work with your local Avnet FAE to see if we will have a Mini-Module Plus that fits your needs.  These are intended to be integrated into commercial products.  See http://em.avnet.com/k7mmp as an example of the form factor and development platform.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bhfletcher

    Thank you very much for the quick reply Bryan.

    I very much like the concept of the Mini-module plus system, though we were specifically looking for a board based on the Zynq processor, do you know if there are any plans for such? (Unfortunately, I had previously attempted to contact my local Avnet FAE regarding this very issue and received no response).
    It is good to know that those modules can be used in a commercial application, I thought they might have the same restrictions as the Xilinx Development kits, being also listed as development.

    I was intrigued by the customisation options specified in the linked thread, however I thought that for a use where the Zedboard would suffice, the cost would be quite prohibitive for a limited run, probably between 100-500 items, that is if it's possible to use it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bhfletcher

    Thank you very much for the quick reply Bryan.

    I very much like the concept of the Mini-module plus system, though we were specifically looking for a board based on the Zynq processor, do you know if there are any plans for such? (Unfortunately, I had previously attempted to contact my local Avnet FAE regarding this very issue and received no response).
    It is good to know that those modules can be used in a commercial application, I thought they might have the same restrictions as the Xilinx Development kits, being also listed as development.

    I was intrigued by the customisation options specified in the linked thread, however I thought that for a use where the Zedboard would suffice, the cost would be quite prohibitive for a limited run, probably between 100-500 items, that is if it's possible to use it.