Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Linux on Zynq Lab 0.1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 374 subscribers
  • Views 459 views
  • Users 0 members are here
Related

Linux on Zynq Lab 0.1

e14 Contributor
e14 Contributor over 12 years ago

Apparently, the Sourcery CodeBench install can no longer be downloaded - as referenced in Lab 0.1:page 29 (step 13). What do you recommend as the step forward for working through your labs? I cannot seem to locate a similar download on the Xilinx site.

Thanks,

-D

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 12 years ago

    Hi dirvin,

    My colleague pointed out that I was not very clear about what needs to be done in order to get the cross compiler installed on your system.

    The best way to get the compiler installed on your Linux system is to perform a full install of the ISE + SDK tools on your Linux system. 

    If you are not already familiar with installing the Xilinx tools under Linux, Xilinx has some documentation which covers the tools installation process for both Windows and Linux which you may find useful, here is one for the ISE 14.5 tools:

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx14_5/irn.pdf

    Once the ISE tools are installed onto your Linux system, your path can be setup to add the tool chain folder to the command search path so that the Sourcery CodeBench cross compiler referred to in the SpeedWay instructions is supplanted by the version which is included with the ISE tools install.  The tool chain included in the ISE install can be used to build the kernel and applications used in the remainder of the SpeedWay labs.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 12 years ago

    Hi dirvin,

    My colleague pointed out that I was not very clear about what needs to be done in order to get the cross compiler installed on your system.

    The best way to get the compiler installed on your Linux system is to perform a full install of the ISE + SDK tools on your Linux system. 

    If you are not already familiar with installing the Xilinx tools under Linux, Xilinx has some documentation which covers the tools installation process for both Windows and Linux which you may find useful, here is one for the ISE 14.5 tools:

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx14_5/irn.pdf

    Once the ISE tools are installed onto your Linux system, your path can be setup to add the tool chain folder to the command search path so that the Sourcery CodeBench cross compiler referred to in the SpeedWay instructions is supplanted by the version which is included with the ISE tools install.  The tool chain included in the ISE install can be used to build the kernel and applications used in the remainder of the SpeedWay labs.

    Regards,

    -Kevin