Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Linux startup hangs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 373 subscribers
  • Views 870 views
  • Users 0 members are here
Related

Linux startup hangs

e14 Contributor
e14 Contributor over 12 years ago

When starting linux for the first time. I get to the following point and then the process hangs:



U-Boot 2011.06 (Sep 03 2012 - 18:38:45)
Xilinx Zynq Platform

DRAM:  512 MiB
MMC:   SDHCI: 0
SF: Got idcode 01 02 19 4d 01
SF: Detected S25FL256S_64K with sector size 64 KiB, total 32 MiB
*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
*** Warning - Setting up bootcmd based on boot mode jumper

Net:   XGem.e000b000
U-BOOT for Avnet-Digilent-ZEDBoard-GTS-14.2

Resetting PHY...

PHY reset complete.

Waiting for PHY to complete autonegotiation.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 12 years ago

    Hi foy,

    Are you attempting to boot with an Ethernet cable connected between ZedBoard and a PC? 

    You should not need a network connection to boot ZedBoard but if you are attempting with a cable connection I wonder if there is a hangup during auto-negotiation with the remote host.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 12 years ago

    Hi foy,

    Are you attempting to boot with an Ethernet cable connected between ZedBoard and a PC? 

    You should not need a network connection to boot ZedBoard but if you are attempting with a cable connection I wonder if there is a hangup during auto-negotiation with the remote host.

    Regards,

    -Kevin