Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Not able to boot Linux from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 374 subscribers
  • Views 1236 views
  • Users 0 members are here
Related

Not able to boot Linux from SD card

e14 Contributor
e14 Contributor over 11 years ago

Hi all,

I am trying to boot Linux from SD card on a Zedboard rev C. I'm able to successfully boot Linux using the files provided with the Zedboard (OOB design), but not with those generated by PetaLinux. I know for sure that the image created by PetaLinux works correctly as I have used it many times on a different Zedboard. I have also checked that all the jumpers are in the correct position.

Any ideas or suggestions?


Thanks,

David

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I will ask our SW guys about PetaLinux version 2014.2.

     

    All rev D Zedboards have production silicon. I suppose it is possible that some rev C Zedboards are not ES silicon. You could check the silicon rev for both of your rev C ZedBoards and see if they are the same. Per UG585, the Zynq TRM (http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf ) on page 1160, you can read the MCTRL register and retrieve the silicon rev.

     

    To read the MCTRL Launch an XMD console in SDK and then connect to the ARM  "connect arm hw" and then read the register with a memory read command "mrd 0xF8007080".  The MS 4 bits are the silicon rev. Rev 3 or higher (0x2 or 0x3) is production silicon.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I will ask our SW guys about PetaLinux version 2014.2.

     

    All rev D Zedboards have production silicon. I suppose it is possible that some rev C Zedboards are not ES silicon. You could check the silicon rev for both of your rev C ZedBoards and see if they are the same. Per UG585, the Zynq TRM (http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf ) on page 1160, you can read the MCTRL register and retrieve the silicon rev.

     

    To read the MCTRL Launch an XMD console in SDK and then connect to the ARM  "connect arm hw" and then read the register with a memory read command "mrd 0xF8007080".  The MS 4 bits are the silicon rev. Rev 3 or higher (0x2 or 0x3) is production silicon.

     

    -Gary