Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Speedway Lab 10 Difficulties
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 374 subscribers
  • Views 439 views
  • Users 0 members are here
Related

Speedway Lab 10 Difficulties

e14 Contributor
e14 Contributor over 10 years ago

Is anyone doing Lab 10 of the Speedway SW series and encountering the undefined value XPAR_FABRIC_PWM_W_INT_0_INTERRUPT_OUT_INTR in the examples? I have a complier error on this value that doesn't seem to be defined anywhere in the entire workspace.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I ran into the same problem using Vivado 2016.2, and here's what I did to fix it:

    The HW Block Diagram shows the PWM_w_Int_0 module's "Interrupt_out" net connected to the Zynq module's "IRQ_F2P[0:0]" port. From the Xilinx documentation I note that IRQ_F2P[0] is Interrupt ID 61, which is #define'd in xparameters_ps.h as "XPS_FPGA0_INT_ID". So I added a #include "xparameters_ps.h" to the top of my LED_Dimmer_Int.c file, and changed the #define INTC_PWM_INTERRUPT_ID to set it to XPS_FPGA0_INT_ID.

    Of course you could alternately short-circuit the extra #include by simply directly setting XPS_FPGA_INT_ID to 61.

    If there's a more "official" way to pass interrupt assignments via the hardware definition I'd love to know!

    - Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I ran into the same problem using Vivado 2016.2, and here's what I did to fix it:

    The HW Block Diagram shows the PWM_w_Int_0 module's "Interrupt_out" net connected to the Zynq module's "IRQ_F2P[0:0]" port. From the Xilinx documentation I note that IRQ_F2P[0] is Interrupt ID 61, which is #define'd in xparameters_ps.h as "XPS_FPGA0_INT_ID". So I added a #include "xparameters_ps.h" to the top of my LED_Dimmer_Int.c file, and changed the #define INTC_PWM_INTERRUPT_ID to set it to XPS_FPGA0_INT_ID.

    Of course you could alternately short-circuit the extra #include by simply directly setting XPS_FPGA_INT_ID to 61.

    If there's a more "official" way to pass interrupt assignments via the hardware definition I'd love to know!

    - Richard