Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Linux + FPGA on the zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 374 subscribers
  • Views 2293 views
  • Users 0 members are here
Related

Linux + FPGA on the zedboard

e14 Contributor
e14 Contributor over 14 years ago

The Zedboard seems very interesting, it has an ARM processor on which a user can run a linux system, it is tightly coupled to an FPGA, and it includes several peripherals and an FMC connector. 

I plan to run linux on the zedboard, and I want to stick the zedboard on a network and access the zedboard remotely using an ethernet connection, will that just work?

OK next, I want to create an FPGA application, I will want to use an external clock, is there an input for that?  I also want to use an external trigger input, do I use the XADC for that?  What is the XADC?

How about moving data back and forth between linux and the FPGA, what will be involved to make that work?

Thanks.



  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi, I was wondering if I could get some info on internet connection using ethernet socket.

    I am planning to connect or send a HTTP package or some sort of data to my FPGA (or ARM processor) on zedboard via internet. I would like to know if linux kernel unpacks this received package for me. In other words, how having a zedboard can help me to send data from internet to my board, and eventually updating some of the register?

    I hope I was clear enough.

    I truly appreciate your help in advance, any type of instructions or steps that can help me in overcoming this issue is tremendously appreciated.



    Sincerely,
    Daniel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi, I was wondering if I could get some info on internet connection using ethernet socket.

    I am planning to connect or send a HTTP package or some sort of data to my FPGA (or ARM processor) on zedboard via internet. I would like to know if linux kernel unpacks this received package for me. In other words, how having a zedboard can help me to send data from internet to my board, and eventually updating some of the register?

    I hope I was clear enough.

    I truly appreciate your help in advance, any type of instructions or steps that can help me in overcoming this issue is tremendously appreciated.



    Sincerely,
    Daniel