Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Linux + FPGA on the zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 374 subscribers
  • Views 2293 views
  • Users 0 members are here
Related

Linux + FPGA on the zedboard

e14 Contributor
e14 Contributor over 14 years ago

The Zedboard seems very interesting, it has an ARM processor on which a user can run a linux system, it is tightly coupled to an FPGA, and it includes several peripherals and an FMC connector. 

I plan to run linux on the zedboard, and I want to stick the zedboard on a network and access the zedboard remotely using an ethernet connection, will that just work?

OK next, I want to create an FPGA application, I will want to use an external clock, is there an input for that?  I also want to use an external trigger input, do I use the XADC for that?  What is the XADC?

How about moving data back and forth between linux and the FPGA, what will be involved to make that work?

Thanks.



  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Great, thanks for the excellent and quick reply!

    Any chance that we can get some simple linux reference designs that use AXI4 to go between the ARM/Linux and the FPGA I/O?   For example the user presses buttons on the Zedboard and data appears on the linux side or the user writes to a file on the linux side and controls LED's on the Zedboard?


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    These example projects are in the works, and should be posted shortly.  Stay tuned!  I'll post back here as soon as they are posted as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Are any of these projects available yet? I am also interested in creating a driver to talk to the FPGA logic from Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Are any of these projects available yet? I am also interested in creating a driver to talk to the FPGA logic from Linux.