Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Linux + FPGA on the zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 374 subscribers
  • Views 2293 views
  • Users 0 members are here
Related

Linux + FPGA on the zedboard

e14 Contributor
e14 Contributor over 14 years ago

The Zedboard seems very interesting, it has an ARM processor on which a user can run a linux system, it is tightly coupled to an FPGA, and it includes several peripherals and an FMC connector. 

I plan to run linux on the zedboard, and I want to stick the zedboard on a network and access the zedboard remotely using an ethernet connection, will that just work?

OK next, I want to create an FPGA application, I will want to use an external clock, is there an input for that?  I also want to use an external trigger input, do I use the XADC for that?  What is the XADC?

How about moving data back and forth between linux and the FPGA, what will be involved to make that work?

Thanks.



  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    There are three questions in your post. The answer is "yes" to all.

    Yes, the zedboard can run web server software. The demo system runs Linux and, I believe, also includes the Apache web daemon. In general, almost every existing Linux app can be built to run on the zedboard. A web server is special only in that the standard package already includes it.

    You can write your own software to interact with the FPGA system.

    And last, your web page can call your software to control your hardware.

    Good luck, and have fun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    There are three questions in your post. The answer is "yes" to all.

    Yes, the zedboard can run web server software. The demo system runs Linux and, I believe, also includes the Apache web daemon. In general, almost every existing Linux app can be built to run on the zedboard. A web server is special only in that the standard package already includes it.

    You can write your own software to interact with the FPGA system.

    And last, your web page can call your software to control your hardware.

    Good luck, and have fun.