Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SD card content invisible
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 310 views
  • Users 0 members are here
Related

SD card content invisible

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I have a microzed board that works really well. The SDK is installed on my laptop, it boots nicely from the QSPI flash and subsequently from the SD card, ending up with a Linux version 3.8.0 kernel + a functional shell. Downloading and executing applications works equally fine.

The only odd thing is that when I insert the micro SD card in the SD card adapter and put that into my PC I do not see a single file on the SD card, no boot image: just nothing at all.
Stick the micro SD card back in the Microzed micro SD slot and run the board again, sure enough: everything is perfect again.

Reading a FAT32 formatted SD card should be no problem at all for a standard WIN7 PC or am I missing something ?

Any help/suggestion much appreciated.



  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Scratch transmission, I had a closer look at the documentation and the SD card being empty is standard.
    I was confused because when the board boots with or without an SD card there is a slight difference. Without an SD card you get a few error messages that basically say: I tried to mount the SD card but I could not find it. With an SD card you get a few messages saying it was able to mount the SD card.

    Once you know it is glaringly obvious.