Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General About ZedBoard's SD card interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 801 views
  • Users 0 members are here
Related

About ZedBoard's SD card interface

e14 Contributor
e14 Contributor over 14 years ago

  I am making a PS configration of ZED by ISE 14.1. For SD card interface, the HW User's Guide and the schematic both use MIO[40..47] . But in XPS tools, only find MIO[40..45] when enable SD0. The MIO[46..47] are used for UART0. Why?
 
  BTW, about zynq chip model,HW user's Guide is XC7Z020-1CSG484.However, Schematic is XC7Z020-1CLG484. Any difference?

Fermi

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Fermi,

    Xilinx moved to the CLG package for better signal integrity.  The Users Guide was written before the change.  I will pass along the recommendation to change it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    In my XPS tools, I find MIO[40...47] are use for SD0.Do you use the ZC702 Development Board Template?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 14 years ago

    Fermi,

    There are 6 primary SD connections, which is what you see with MIO[40:45].  If you click the + (plus) sign in front of the SD peripheral, you'll find optional connections for WP, CD, and Power.  On ZedBoard, we connect WP to MIO[46] and CD to MIO[47].  Note that the location of the primary and optional connections all have some flexibility. 

    ZC702 uses the same MIO[40:45] for the primary connections, but CD is connected to MIO[0] and WP is at MIO[15].

    I found one additional stray reference to the CSG package in the HW UG (on Figure 1 Block Diagram).  We are using the CLG package and will get this typo corrected soon.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    minm,

    You may find this blog post helpful:

    http://zynqgeek.blogspot.com/2012/08/zedboard-create-planahead-project-with.html