Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General booting problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 373 subscribers
  • Views 566 views
  • Users 0 members are here
Related

booting problem

e14 Contributor
e14 Contributor over 10 years ago

sir when i am booting the zedboard it is struct at this position

U-Boot 2014.01 (Apr 19 2016 - 09:36:36)

I2C: ready
Memory: ECC disabled
DRAM: 512 MiB
MMC: zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
*** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial
Net: Gem.e000b000
Hit any key to stop autoboot: 0
Device: zynq_sdhci
Manufacturer ID: 83
OEM: 4e43
Name: NCard
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 29.5 GiB
Bus Width: 4-bit
reading uEnv.txt
** Unable to read file uEnv.txt **
Copying Linux from SD to RAM...
reading uImage
3724512 bytes read in 356 ms (10 MiB/s)
reading devicetree.dtb
9769 bytes read in 16 ms (595.7 KiB/s)
## Booting kernel from Legacy Image at 03000000 ...
Image Name: Linux-4.4.0-xilinx-g3c07939-dirt
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3724448 Bytes = 3.6 MiB
Load Address: 00008000
Entry Point: 00008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 02a00000
Booting using the fdt blob at 0x2a00000
Loading Kernel Image ... OK
Loading Device Tree to 1fb29000, end 1fb2e628 ... OK

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.4.0-xilinx-g3c07939-dirty (root@linux32) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5) ) #7 SMP PREEMPT Mon May 2 09:32:12 IST 2016
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Zynq Zed Development Board
cma: Reserved 16 MiB at 0x1e800000
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @5fbce000 s19328 r8192 d21632 u49152
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttyPS0,115200n8 root=/dev/ram rw initrd=0x00800000,16M earlyprintk mtdparts=physmap-flash.0:512K(nor-fsbl),512K(nor-u-boot),5M(nor-linux),9M(nor-user),1M(nor-scratch),-(nor-rootfs)
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 479228K/524288K available (5091K kernel code, 207K rwdata, 1788K rodata, 256K init, 224K bss, 28676K reserved, 16384K cma-reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0x60800000 - 0xff800000 (2544 MB)
lowmem : 0x40000000 - 0x60000000 ( 512 MB)
pkmap : 0x3fe00000 - 0x40000000 ( 2 MB)
modules : 0x3f000000 - 0x3fe00000 ( 14 MB)
.text : 0x40008000 - 0x406bff30 (6880 kB)
.init : 0x406c0000 - 0x40700000 ( 256 kB)
.data : 0x40700000 - 0x40733e60 ( 208 kB)
.bss : 0x40733e60 - 0x4076bf34 ( 225 kB)
Preemptible hierarchical RCU implementation.
Build-time adjustment of leaf fanout to 32.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
slcr mapped to 60800000
L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 1 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 8 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
zynq_clock_init: clkc starts at 60800100
Zynq clock init
sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
timer #0 at 60808000, irq=17
Console: colour dummy device 80x30
Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x8280 - 0x82d8
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (2664.03 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x60880000
zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
media: Linux media interface: v0.10
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
EDAC MC: Ver: 3.0.0
Advanced Linux Sound Architecture Driver Initialized.
clocksource: Switched to clocksource arm_global_timer
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (junk in compressed archive); looks like an initrd
Freeing initrd memory: 16384K (40800000 - 41800000)
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
futex hash table entries: 512 (order: 3, 32768 bytes)
jffs2: version 2.2. (NAND) (SUMMARY) u00A9 2001-2006 Red Hat, Inc.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
dma-pl330 f8003000.dmac: DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 143, base_baud = 3125000) is a xuartps
console [ttyPS0] enabled
xdevcfg f8007000.devcfg: ioremap 0xf8007000 to 6086c000
[drm] Initialized drm 1.1.0 20060810
brd: module loaded
loop: module loaded
m25p80 spi0.0: found s25fl256s1, expected n25q128a11
m25p80 spi0.0: s25fl256s1 (32768 Kbytes)
5 ofpart partitions found on MTD device spi0.0
Creating 5 MTD partitions on "spi0.0":
0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
0x000000100000-0x000000600000 : "qspi-linux"
0x000000600000-0x000000620000 : "qspi-device-tree"
0x000000620000-0x000000c00000 : "qspi-rootfs"
0x000000c00000-0x000001000000 : "qspi-bitstream"
CAN device driver interface
libphy: MACB_mii_bus: probed
macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 146 (00:0a:35:00:01:22)
macb e000b000.ethernet eth0: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=e000b000.etherne:00, irq=-1)
e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
usbcore: registered new interface driver usb-storage
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver

its struct at this position

please suggest me any idea

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi babuji,

    This sort of condition is usually caused by some sort of driver mismatch to the hardware platform.  This could be due to a device tree entry that does not correctly line up to hardware implemented on the PS or even in PL memory space.

    Looking at the date stamp of the U-Boot build, it looks like you are trying to build this yourself.

    My recommendation would be to take something that is known to work, like one of the Xilinx official releases and see how your build differs from that.

    http://www.wiki.xilinx.com/Zynq+Releases

    You can then divide and conquer to see what changes cause Linux to no longer boot in order to isolate what entry is causing the problem.

    Unfortunately, that process can be time consuming but if you need to build older 2014.1 components, that may be your only option at this point.

    Regards,

    -Kevin