Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard connecting 7segment displayer
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 1381 views
  • Users 0 members are here
Related

Zedboard connecting 7segment displayer

e14 Contributor
e14 Contributor over 11 years ago

Hello,
I was wondering whether it is possible to connect a 4x7-segment led displayer to Zedboard for simple multiplexing purposes. If so please be so kind and explain a little bit of it, I'm totally new to Zedboard.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Conceptually what you describe should be OK. By my count, since JA-5 is ground and JA-6 is 3.3VDC, you will need to use two more signals on the JB connector. There are no electrical specification with the diagram you link to, so you will need to make sure that you do not exceed the voltage and current limits for the Zynq I/O configured as LVCMOS33 with your circuit. The Zynq 7020 data sheet is available here: http://www.xilinx.com/support/documentation/data_sheets/ds187-XC7Z010-XC7Z020-Data-Sheet.pdf

     

    You will need to set your constraints to set the Zynq IO to LVCMOS33. And, since the PMOD IO are directly connected to the Zynq device, you will need to take normal precautions to prevent damage from static discharge or overvoltage conditions.

     

    As a reference Digilent does make a PMOD 7-segment LED display module: http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,401,481&Prod=PMOD-SSD

     

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Conceptually what you describe should be OK. By my count, since JA-5 is ground and JA-6 is 3.3VDC, you will need to use two more signals on the JB connector. There are no electrical specification with the diagram you link to, so you will need to make sure that you do not exceed the voltage and current limits for the Zynq I/O configured as LVCMOS33 with your circuit. The Zynq 7020 data sheet is available here: http://www.xilinx.com/support/documentation/data_sheets/ds187-XC7Z010-XC7Z020-Data-Sheet.pdf

     

    You will need to set your constraints to set the Zynq IO to LVCMOS33. And, since the PMOD IO are directly connected to the Zynq device, you will need to take normal precautions to prevent damage from static discharge or overvoltage conditions.

     

    As a reference Digilent does make a PMOD 7-segment LED display module: http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,401,481&Prod=PMOD-SSD

     

     

    -Gary