Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard connecting 7segment displayer
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 1380 views
  • Users 0 members are here
Related

Zedboard connecting 7segment displayer

e14 Contributor
e14 Contributor over 11 years ago

Hello,
I was wondering whether it is possible to connect a 4x7-segment led displayer to Zedboard for simple multiplexing purposes. If so please be so kind and explain a little bit of it, I'm totally new to Zedboard.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Let me be more specific, I got 2 of these
    http://www.tandyonline.co.uk/media/wysiwyg/276-078-Two-Digit-7-Segment-Display-pins.png
    So I have 4 digits and I want to use multiplexing, what I came up with is D1(a) D2(a) D3(a) D4(a) tied up together and same for other segments, it gives 8 bits required + 4 bits for common cathodes. The question is whether I can use JA1-JA10 + JB1-JB2 to be inputs for diodes in series with resistors and an output for common cathodes? To lower the current I can use bipolar transistors and control their bases, current for the base is then about 0,05mA. Is it a appropriate solution for connecting this led displayer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Let me be more specific, I got 2 of these
    http://www.tandyonline.co.uk/media/wysiwyg/276-078-Two-Digit-7-Segment-Display-pins.png
    So I have 4 digits and I want to use multiplexing, what I came up with is D1(a) D2(a) D3(a) D4(a) tied up together and same for other segments, it gives 8 bits required + 4 bits for common cathodes. The question is whether I can use JA1-JA10 + JB1-JB2 to be inputs for diodes in series with resistors and an output for common cathodes? To lower the current I can use bipolar transistors and control their bases, current for the base is then about 0,05mA. Is it a appropriate solution for connecting this led displayer?