Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zynq intro/ LAb 3 "Error detect phy"
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 372 subscribers
  • Views 864 views
  • Users 0 members are here
Related

Zynq intro/ LAb 3 "Error detect phy"

e14 Contributor
e14 Contributor over 13 years ago

Hi!

I have a problem with Lab3 and was wondering if someone could help me please. I keep running in this error in Lab3/ Peripheral Test: "Error detect phy"

the full output when launchig that test is:

---Entering main---

Running ScuGicSelfTestExample() for ps7_scugic_0...
ScuGicSelfTestExample PASSED
ScuGic Interrupt Setup PASSED

Running Interrupt Test  for ps7_ethernet_0...
Error detect phy

there is nothing happening afterwards.

i also tested this with the solution to lab 3 and there is the same error message and the exact same behaviour. Could someone please tell me waht is going on? is my board broken or is this another problem?

I'm running Xilinx 14.4 toolchain.

Regards,
milchprodukt

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    thanks for your quick reply, it is working now.

    But if I understand this rght what i did now is overwriting my own peripheral config with a premade one, right? how can i find out what was wrong with my own config?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I'm also using Xilinx ISE 14.4 and running the Zynq Intro.
    Just like you, I am getting the same problem with the peripheral tests on Lab3

    The Hello World and Memory tests work. However Peripheral test fails on the Ethernet with the message:
    *Running Interrupt Test  for ps7_ethernet_0...
    *Error detect phy
    and stops there.

    If I comment out this Ethernet test from the main, all the remaining tests complete with PASSED, except for the QPSI test:
    *Running QspiSelfTestExample() for ps7_qspi_0...
    *QspiPsSelfTestExample FAILED

    I tried many things, including using the backup Lab3, rebooting, various builds, and removing other applications, all without success.
    I will now try the proposed fix above, that I just found.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I sure wish I knew why. This approach failed 20 times for me yesterday in every variation. Today, I just started up PlanAhead from the ISE command line, went to SDK by the "Export Hardware for SDK" and this time I just selected Launch SDK and unselected "Export Hardware". In SDK, I selected the peripheral_tests_0 and from the RMB selected "Run As | Launch on Hardware".

    Two peripherals that didn't work yesterday now test fine:

    Running Interrupt Test  for ps7_ethernet_0...
    EmacPsDmaIntrExample PASSED

    Running QspiSelfTestExample() for ps7_qspi_0...
    QspiPsSelfTestExample PASSED

    Maybe the overnight reboot of my computer, as well as power off the zedboard is what helped? I'd test cycled the power on the zedboard in my earlier fails, so maybe it was my computer reboot somehow? Very puzzled as to why it works now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,
    I'm try to run the labs using Vivado and I'm having the same problem. I've already imported the preset configuration for the zedboard, but I still have the "Error detect phy" message

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I had the same problem, but after power cycling the zedboard it worked fine ;)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    +1 for this comment -- I had the same problem and power cycling fixed it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Me TOO, same problem and same solution