Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Linux stop boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 480 views
  • Users 0 members are here
Related

Linux stop boot

e14 Contributor
e14 Contributor over 11 years ago

Hi,



I configured my SD for my Zedboard in order to run Linux. The bootloader load the kernel but the kernel don't load Linux. I followed the tutoriel provided by the Zedboard Website (tutorial's name is : Ubuntu Desktop Linux). In hyperterminal (TeraTerm) I have this :



U-Boot 2015.01 (May 06 2015 - 16:36:20)

Board:  Xilinx Zynq
I2C:   ready
DRAM:  ECC disabled 512 MiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
In:    serial
Out:   serial
Err:   serial
Board:  Xilinx Zynq
Net:   Gem.e000b000
Hit any key to stop autoboot:  0
Device: zynq_sdhci
Manufacturer ID: 27
OEM: 5048
Name: SD04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading uEnv.txt
** Unable to read file uEnv.txt **
Copying Linux from SD to RAM...RFS in ext4
reading uImage
2680760 bytes read in 243 ms (10.5 MiB/s)
reading devicetree.dtb
7019 bytes read in 17 ms (402.3 KiB/s)
## Booting kernel from Legacy Image at 02080000 ...
   Image Name:   Linux-3.6.0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2680696 Bytes = 2.6 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 02000000
   Booting using the fdt blob at 0x2000000
   Loading Kernel Image ... OK
   Loading Device Tree to 1ed1e000, end 1ed22b6a ... OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0
Linux version 3.6.0 (root@jordan) (gcc version 4.9.1 (Sourcery CodeBench Lite 2014.11-30) ) #1 SMP PREEMPT Thu May 7 14:27:23 CEST 2015
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED
bootconsole [earlycon0] enabled
cma: CMA: reserved 40 MiB at 1c400000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 7 pages/cpu @c0e50000 s7872 r8192 d12608 u32768
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 512MB = 512MB total
Memory: 468100k/468100k available, 56188k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc04c5468   (4854 kB)
      .init : 0xc04c6000 - 0xc04edec0   ( 160 kB)
      .data : 0xc04ee000 - 0xc053e660   ( 322 kB)
       .bss : 0xc053e684 - 0xc0a456d0   (5149 kB)







Thanks

Jo

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

    I followed all the step. I put boot.bin, devicetree.dtb and uImage in the FAT partition and Linaro RFS in the ext4 partition but the boot already stop.

    Jo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

    I followed all the step. I put boot.bin, devicetree.dtb and uImage in the FAT partition and Linaro RFS in the ext4 partition but the boot already stop.

    Jo