Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General How do I login to Pulsar Linux on Microzed?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 1121 views
  • Users 0 members are here
Related

How do I login to Pulsar Linux on Microzed?

shanedora
shanedora over 7 years ago

I just booted the pulsar linux image that came with my microzed board. I went ahead and setup minicom so I could see the boot process. My host computer is a laptop running CentOS 7 (NOT WINDOWS). It's giving me a login prompt as such...

cube-10-12-15-cube-server login:

On the pulsar linux getting started guide it says to use the credials at the login prompt

root:incendia

Minicom doesn't let me type in anything. So how am I suppose to log in to it? Where are these instructions at? Can I setup a ssh session and if so where are the instructions for this? Direct links much appreciated in setting up a ssh session.

A few restrictions are...

I cannot plug this board into a modem. I need to plug the zed into my laptop which is connected to wifi.

~S

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 7 years ago

    Hello scy86dev,

    Was your MicroZed shipped with Pulsar Linux?  Was the MicroZed purchased recently?  The reason I ask is that we  do not directly support Wind River Pulsar Linux from our side anymore and so I did not think we were shipping SD cards with it loaded anymore either.

    The quickest way to get to a command prompt is to go through the serial terminal as you are doing.  These threads may be helpful in getting your serial terminal working:

    http://microzed.org/content/usb-uart-problem

    http://microzed.org/content/microzed-cant-get-hello-world-print-anything-consoleminicom

    I don't think you will need a modem for the board, although you may want to use wired Ethernet on MiniZed to connect to your network.

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 7 years ago

    Hello scy86dev,

    Was your MicroZed shipped with Pulsar Linux?  Was the MicroZed purchased recently?  The reason I ask is that we  do not directly support Wind River Pulsar Linux from our side anymore and so I did not think we were shipping SD cards with it loaded anymore either.

    The quickest way to get to a command prompt is to go through the serial terminal as you are doing.  These threads may be helpful in getting your serial terminal working:

    http://microzed.org/content/usb-uart-problem

    http://microzed.org/content/microzed-cant-get-hello-world-print-anything-consoleminicom

    I don't think you will need a modem for the board, although you may want to use wired Ethernet on MiniZed to connect to your network.

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • shanedora
    0 shanedora over 7 years ago in reply to zedhed

    Kevin ~ I'm assuming you're the same Kevin that replied to the posts you mentioned above on adding udev rules? If so, would you be so kind to help me understand a few udev settings you made....

    ENV{ID_MM_DEVICE_IGNORE}="1"
    You mentioned you did this to prevent the modem manager from touching the USB-UART device that is the target board. I guess I don't understand what the modem manager is and when it's appropriate to ensure it's ignore. I googled "Modem Manager" a bit but most tutorials were alittle above my head to grasp the full picture of it's purpose.

    sudo usermod -a -G dialout AES_CM
    Who and where did this AES_CM user come from? I've never heard of such as user. Exteremely confused what this is. I thought I only need to add myself (my user account i log in with) to the dialout group?

    ATTR{idVendor} and the ATTR{idProduct}
    How did you find these two attributes from the command line? Would you be so kind to show me how I can determine these two values? Also you matched these keys to idVendor being "04b4" and idProduct being "0008". What if my MicroZed board has different vendor and product id's? Will they? This is why I ask in how I can effectively determine what the two are myself.