Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Relation between vivado and yocto on zedboard?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 375 subscribers
  • Views 602 views
  • Users 0 members are here
Related

Relation between vivado and yocto on zedboard?

e14 Contributor
e14 Contributor over 9 years ago

Dear, 

I've followed architect's guide (http://architechboards-zedboard.readthedocs.io/en/latest/index.html) to install yocto, and now i have yocto running on zedboard.

Now I have 2 problems:

1- When I program the fpga from vivado or sdk  the yocto seems freezing, as the terminal throug usb uart becomes inactive, any idea why and how can I program fpga and keep yocto running?

2- how to create an application in vivad sdk which targeting yocto, so that the elf file will run on yocto?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Jhonnylamma,

    You seem to be a bit confused in regards to how you are programming your Zedboard. When you say you are programming your ZedBoard by USB  I believe you mean USB-JTAG. The JTAG connector is pre built into your ZedBoard at the J17 Micro B USB connector. See page 12 of the "ZedBoard Hardware User Guide".

    http://zedboard.org/support/documentation/1521

    So when you plug your USB cable into J17, you are indeed using USB-JTAG to program your board. JTAG is one of 3 boot (programming) methods offered on Zedboard. The other two are QSPI and SD card boot. JTAG is stored in volatile memory while QSPi and SD Card boot are both non-volatile memory.

    As you seem relatively new to Zynq develpoment, am going to suggest you go through our Developing Zynq Software Speedway course.

    http://zedboard.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-201441-20152-and-20162

    This will help you obtain a better understanding of how all the different boot/programming methods work.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Jhonnylamma,

    You seem to be a bit confused in regards to how you are programming your Zedboard. When you say you are programming your ZedBoard by USB  I believe you mean USB-JTAG. The JTAG connector is pre built into your ZedBoard at the J17 Micro B USB connector. See page 12 of the "ZedBoard Hardware User Guide".

    http://zedboard.org/support/documentation/1521

    So when you plug your USB cable into J17, you are indeed using USB-JTAG to program your board. JTAG is one of 3 boot (programming) methods offered on Zedboard. The other two are QSPI and SD card boot. JTAG is stored in volatile memory while QSPi and SD Card boot are both non-volatile memory.

    As you seem relatively new to Zynq develpoment, am going to suggest you go through our Developing Zynq Software Speedway course.

    http://zedboard.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-201441-20152-and-20162

    This will help you obtain a better understanding of how all the different boot/programming methods work.

    --Josh