Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Interrupt not working properly
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 373 subscribers
  • Views 291 views
  • Users 0 members are here
Related

Interrupt not working properly

e14 Contributor
e14 Contributor over 10 years ago

Hey,

I'm currently working on my master thesis where I have to implement a domain specific DMA controller in VHDL.

Here everything's working fine. But I have a problem at handling interrupts coming from my custom DMAC IP. At the beginning I have to configure my DMAC via AXI Lite and have to give him a transaction table that it can process. Then I enable the DMAC. Before this all is done I want to setup the interrupt stuff, so that I get an interrupt as soon as all transfers are processed.

The problem is, that the assigned interrupt service routine is not executed if I do it in this order. Here the program simply stops if the interrupt occurs. Only if I setup the IRQ after the DMAC is enabled (and some extra delay between...), the ISR is called and the IRQ is acknowledged. Here is the code I want to be processed:
 

//SCUGIC interrupt controller Intialization
//Registration of the ISR
xStatus = initializeInterruptSystem(XPAR_PS7_SCUGIC_0_DEVICE_ID);
if(XST_SUCCESS != xStatus)
      print(" :( SCUGIC INIT FAILED \n\r");

/* Here the configuration of the DMAC is done */
.....
/* End of the configuration */

// enabling the DMAC
Xil_Out32(DMA2_CONFIG_BASEADDR + 0 * 0x4, 1);


But it's only working if I do it like this:


/* Here the configuration of the DMAC is done */
.....
/* End of the configuration */

// enabling the DMAC
Xil_Out32(DMA2_CONFIG_BASEADDR + 0 * 0x4, 1);

// extra delay ...
int ctr = 0;
for (ctr = 0; ctr < 100; ++ctr);

//SCUGIC interrupt controller Intialization
//Registration of the ISR
xStatus = initializeInterruptSystem(XPAR_PS7_SCUGIC_0_DEVICE_ID);
if(XST_SUCCESS != xStatus)
    print(" :( SCUGIC INIT FAILED \n\r");


The initializeInterruptSystem(...) routine is implemented like in http://www.xilinx.com/support/answers/50572.html.


I hope you have an idea of what's wrong here.


Pascal

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hellow Pascal,

     

    There is an example of implementing a custom IP with interrupts in Lab 7 of the Avnet Zynq 7000 Hardware Speedway workshop. In Lab 10 of the Avnet Zynq 7000 Software Speedway workshop there is an example of using this custom IP, including the interrupts, in the SDK.

    Take a look at these examples and see how the interrupts are initialized and used. The Speedway workshops can be downloaded here:

    http://zedboard.org/support/trainings-and-videos

     

    Adam Taylor also has some posts on using interrupts in his MicroZed Chronicles blog:

    http://zedboard.org/content/microzed-chronicles

     

    -Gary