Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General UltraZed-EG DisplayPort Problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 983 views
  • Users 0 members are here
  • Using Xilinx Tools
  • ZedBoard General Questions
  • ultrazed
  • displayport
  • Zedboard Hardware Design
  • Software Application Development
  • Ultrazed Hardware Design
  • linux
Related

UltraZed-EG DisplayPort Problem

falcon_greatly
falcon_greatly over 7 years ago

Hello,

 

I am trying to work with the DisplayPort on UltraZed IO Carrier Board but I have a problem in Linux Bootup.

I tried binaries posted from Avnet here and it's working on my display with my board.
I tried to use the scripts in Avnet but I failed to build it. I think it's outdated.
I tried to memic the changes in petalinux and hardware changes from the Avnet Repos and I have the following blocking issue:
Can anyone help me on how to fix this issue ?

 

[    6.034827] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:8 protocol:4 pll_locked:yes

[    6.045070] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed

[    6.055692] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed

[    6.063703] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed

[    6.071938] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok

[    6.084291] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok

[    6.096893] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed

[    6.106993] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000

[    6.113928] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

[    6.120464] [drm] No driver support for vblank timestamp query.

[    6.126447] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008ac6b28)

[    6.169516] zynqmp-display fd4a0000.zynqmp-display: Cannot do DMA to address 0x0000000000000000

[    6.178140] swiotlb: coherent allocation failed for device fd4a0000.zynqmp-display size=9216000

[    6.186818] CPU: 2 PID: 58 Comm: kworker/2:1 Not tainted 4.14.0-xilinx-v2018.2 #9

[    6.194272] Hardware name: Avnet UltraZed-3EG (DT)

[    6.199055] Workqueue: events deferred_probe_work_func

[    6.204165] Call trace:

[    6.206600] [<ffffff80080881f0>] dump_backtrace+0x0/0x368

[    6.211980] [<ffffff800808856c>] show_stack+0x14/0x20

[    6.217016] [<ffffff80089ed678>] dump_stack+0x9c/0xbc

[    6.222050] [<ffffff8008457c9c>] swiotlb_alloc_coherent+0x174/0x180

[    6.228301] [<ffffff8008093a6c>] __dma_alloc+0x13c/0x250

[    6.233596] [<ffffff8008555494>] drm_gem_cma_create+0x8c/0x110

[    6.239409] [<ffffff8008562ab8>] xlnx_fbdev_create+0x68/0x230

[    6.245139] [<ffffff800852eeac>] __drm_fb_helper_initial_config_and_unlock+0x1bc/0x3d0

[    6.253038] [<ffffff800852f100>] drm_fb_helper_initial_config+0x40/0x50

[    6.259633] [<ffffff8008562d20>] xlnx_fb_init+0xa0/0x158

[    6.264927] [<ffffff8008562740>] xlnx_bind+0x270/0x298

[    6.270049] [<ffffff8008570828>] try_to_bring_up_master+0x178/0x1d8

[    6.276299] [<ffffff8008570a88>] component_master_add_with_match+0xa0/0xf8

[    6.283156] [<ffffff8008562934>] xlnx_platform_probe+0x1cc/0x1f8

[    6.289146] [<ffffff8008578148>] platform_drv_probe+0x38/0x78

[    6.294875] [<ffffff80085767b0>] really_probe+0x1b8/0x270

[    6.300257] [<ffffff80085769d4>] __device_attach_driver+0xa4/0x110

[    6.306419] [<ffffff8008574b54>] bus_for_each_drv+0x4c/0x98

[    6.311974] [<ffffff80085765a8>] __device_attach+0xb0/0xe8

[    6.317443] [<ffffff8008576b70>] device_initial_probe+0x10/0x18

[    6.323345] [<ffffff8008575ab4>] bus_probe_device+0x94/0xa0

[    6.328900] [<ffffff8008573ac8>] device_add+0x378/0x578

[    6.334108] [<ffffff8008577f44>] platform_device_add+0x124/0x2a8

[    6.340097] [<ffffff8008562294>] xlnx_drm_pipeline_init+0x7c/0x108

[    6.346263] [<ffffff800856cff0>] zynqmp_dpsub_probe+0x100/0x150

[    6.352163] [<ffffff8008578148>] platform_drv_probe+0x38/0x78

[    6.357892] [<ffffff80085767b0>] really_probe+0x1b8/0x270

[    6.363274] [<ffffff80085769d4>] __device_attach_driver+0xa4/0x110

[    6.369437] [<ffffff8008574b54>] bus_for_each_drv+0x4c/0x98

[    6.374992] [<ffffff80085765a8>] __device_attach+0xb0/0xe8

[    6.380460] [<ffffff8008576b70>] device_initial_probe+0x10/0x18

[    6.386363] [<ffffff8008575ab4>] bus_probe_device+0x94/0xa0

[    6.391918] [<ffffff8008575f5c>] deferred_probe_work_func+0x94/0x140

[    6.398256] [<ffffff80080b0c6c>] process_one_work+0x1dc/0x348

[    6.403983] [<ffffff80080b1024>] worker_thread+0x24c/0x488

[    6.409452] [<ffffff80080b67a4>] kthread+0x12c/0x130

[    6.414399] [<ffffff8008084290>] ret_from_fork+0x10/0x18

[    6.419711] zynqmp-display fd4a0000.zynqmp-display: failed to allocate buffer with size 9216000

[    6.428392] zynqmp-display fd4a0000.zynqmp-display: Failed to set initial hw configuration.

[    6.436721] zynqmp-display fd4a0000.zynqmp-display: failed to initialize drm fb

[    6.444184] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0

[    6.452225] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed

 

 

 

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 7 years ago

    Hi Ahmed,

     

    Which version of Xilinx tools are you using to build your hardware design and which version of PetaLinux tools are you using to build your Linux image?

     

    Which scripts are you using to build your platform with?

     

    Best Regards,

     

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • falcon_greatly
    0 falcon_greatly over 7 years ago in reply to zedhed

    Thanks for you support.

    Issue already fixed in Xilinx forums.

    https://forums.xilinx.com/t5/Embedded-Linux/UltraZed-EG-DisplayPort-Problem/m-p/944628

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer