Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Microzed USB configuration for petalinux 2018
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 374 subscribers
  • Views 4389 views
  • Users 0 members are here
  • iiot
  • microzed
  • industrial_iot
  • petalinux
  • usb
  • microzed_iiot
  • zynq-7000 soc
Related

Microzed USB configuration for petalinux 2018

maldata
maldata over 7 years ago

Hi all,

 

I can see many discussions in the forums about getting USB host-mode working on a Microzed (Zynq 7020). In particular, here's a selection of links that I've already read:

 

  • http://zedboard.org/content/usb-host-microzed-petalinux-20172
  • http://zedboard.org/zh-hant/node/8651
  • https://forums.xilinx.com/t5/Embedded-Processor-System-Design/Cannot-get-USB-to-work-on-microzed-7010-with-arch-linux-using/td-p/652816
  • http://zedboard.org/content/access-usb-microzed-board
  • https://forums.xilinx.com/t5/Embedded-Linux/Petalinux-2015-2-1-usb-not-working/td-p/654349
  • https://forums.xilinx.com/t5/Embedded-Linux/USB-works-in-device-mode-but-not-in-host-mode/td-p/679097

 

I've spent a lot of time googling, but have so far not been successful. I'm using Petalinux 2018 and the Zedboard metadata layers to build the image. I added a device tree layer similar to what is presented here: https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/18842272/Zynq+Linux+USB+Device+Driver

 

By itself, that doesn't work. No USB bus is available. However, I changed the bus's "compatible" property and moved "drv-vbus" from the phy to the bus itself, so now I have

 

/ {

    usb_phy0: phy0 {

        compatible = "usb-nop-xceiv";

        #phy-cells = <0>;

        reg = <0xe0002000 0x1000>;

        view-port = <0x170>;

    };

};

 

&usb0 {

    dr_mode = "host";

    usb-phy = <&usb_phy0>;

    drv-vbus;

};

 

When I use this device tree, the USB bus appears to be available:

 

# lsusb

Bus 001 Device 001: ID 1d6b:0002

# dmesg | grep -i usb

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

usb_phy_generic e0002000.phy0: e0002000.phy0 supply vcc not found, using dummy regulator

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

usbcore: registered new interface driver usb-storage

chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

 

However, the board still does not recognize any USB devices plugged into it. If I plug in a USB flash drive, for example, the LED on the drive does light up, but nothing new is available in lsusb, no new messages appear in dmesg, and no new block device appears in /dev.

 

I've tried everything in the links above, I've tried different USB devices, I've tried a powered USB hub, and all I can figure is that there's still some device between the OS and the port that isn't configured correctly. In particular, I'd like to know more about the following:

 

  • Is there a requirement to toggle the reset on the USB3320 chip after power comes up? I have seen some mention of this in similar posts.
    • Sometimes this is handled by the first-stage bootloader. Can AVnet confirm?
    • If not the first-stage bootloader, does this need to be done some other way?
  • Does USB need to be enabled by setting a GPIO? If so, which GPIO?
  • In older versions of the linux kernel/device tree, a USB PHY configuration was not needed. Now, a PHY element must be added to the device tree in order for the system to recognize the USB root hub. This is not done in the stock Zynq-7000 metadata.
    • Can you confirm that usb-nop-xceiv is appropriate for this PHY?
    • Does the PHY require configuration of clocks or regulators in order to function correctly?
  • When USB devices are inserted, the kernel does not fire uevents. Is there any configuration beyond default that is needed to enable this, or is there a hardware/device tree configuration issue blocking this?
    • In the current configuration, the EHCI is correctly detected
    • Is there any kernel configuration required to ensure that hub IRQs are handled correctly?
    • Is there any kernel configuration required to ensure that hub events are handled correctly?

 

Has anyone managed to get this working on a Microzed, and if so, can you share your method?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • maldata
    0 maldata over 7 years ago

    Here's an update. What I found is that I can start with the vendor BSP, and instead of booting from the ramdisk, I can boot from the rootfs from our PetaLinux project, and the USB port works fine. That rules out the rootfs. Also, the kernel configuration and device tree are pretty much identical to what we produce, so it seems like those are also fine.

     

    The only remaining thing from the BSP then is the BOOT.BIN file. As far as I know, the only things in there are the u-boot executable and the FPGA bitstream, so:

    1. Is there anything at all that may cause u-boot to improperly initialize a device or something?
    2. Is it possible that the FPGA program could somehow cause the USB port to fail?
    3. Is there anything else in BOOT.BIN that I'm not aware of?

     

    I'm still working with the team to determine if there have been any changes to the FPGA since the older, working version.

     

    Thanks,

    -Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • maldata
    0 maldata over 7 years ago

    Here's an update. What I found is that I can start with the vendor BSP, and instead of booting from the ramdisk, I can boot from the rootfs from our PetaLinux project, and the USB port works fine. That rules out the rootfs. Also, the kernel configuration and device tree are pretty much identical to what we produce, so it seems like those are also fine.

     

    The only remaining thing from the BSP then is the BOOT.BIN file. As far as I know, the only things in there are the u-boot executable and the FPGA bitstream, so:

    1. Is there anything at all that may cause u-boot to improperly initialize a device or something?
    2. Is it possible that the FPGA program could somehow cause the USB port to fail?
    3. Is there anything else in BOOT.BIN that I'm not aware of?

     

    I'm still working with the team to determine if there have been any changes to the FPGA since the older, working version.

     

    Thanks,

    -Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • zedhed
    0 zedhed over 7 years ago in reply to maldata

    Hi Mark,

     

    This is some pretty good troubleshooting steps that you have taken so far, it certainly helps narrow down the source of the issue.

     

    Have you done any modifications to the hardware platform in Vivado?

     

    I went back and looked at some old notes and I see this note in the hardware user guide:

     

    6064.contentimage_192677.png

     

    5276-MicroZed-HW-UG-v1-7-V1.pdf

     

    Have you checked the state of the PS_MIO7 signal to make sure that your FSBL within the BOOT.BIN file is not keeping the USB PHY in reset?

     

    Best Regards,

     

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 7 years ago in reply to maldata

    Hi Mark,

     

    I am not sure which pieces you are modifying, but you can use BootGen to recreate the FSBL by using the pre-built fsbl.elf, download.bit, and u-boot.elf files to recreate the BOOT.BIN that is provided as part of the BSP and then use process of elimination to insert your components one at a time into your own custom BOOT.BIN until you see which one breaks.  If the fsbl.elf is the culprit, then I would recommend to check your Viviado design for the correct settings.

     

    I have some further notes here on the HW configuration used by the PetaLinux BSP.

     

    These are the settings we are using for the PS7 block in the Vivado block diagram:

     

    CONFIG.PCW_EN_USB0 {1}

    CONFIG.PCW_USB0_PERIPHERAL_ENABLE {1}

    CONFIG.PCW_USB0_RESET_ENABLE {1}

    CONFIG.PCW_USB0_RESET_IO {MIO 7}

    CONFIG.PCW_USB0_USB0_IO {MIO 28 .. 39}

    CONFIG.PCW_USB_RESET_ENABLE {1}

    CONFIG.PCW_USB_RESET_POLARITY {Active Low}

    CONFIG.PCW_USB_RESET_SELECT {Share reset pin}

     

    If you are modifying the hardware at all using Vivado or making your own hardware platform and then exporting to PetaLinux, please check that your settings match the above settings.

     

    Best Regards,

     

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer