Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Discrepancy on Zedboard Specs Between Zedboard and Xilinx Websites
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 677 views
  • Users 0 members are here
  • zedboard
  • specifications
Related

Discrepancy on Zedboard Specs Between Zedboard and Xilinx Websites

at694
at694 over 7 years ago

Hello,

 

I have a question regarding the Zynq SoC used on the Zedboard.

 

According to the Zedboard website, ZedBoard SDR II Evaluation Kit includes a Zedboard, which according to the specification comes with the Xilinx Zynq SoC XC7Z020-CLG484-1. However, on Xilinx's website, the same kit is quoted to come with the Xilinx Zynq-7000 SoC ZC706.

 

Could someone clear this up for me please?

  • Sign in to reply
  • Cancel
Parents
  • avnrdf
    0 avnrdf over 7 years ago

    It looks like they are different kits to begin with.

     

    The 'SDR II' uses the Zedboard (XC7Z020), but the the 'SDRIII' (or the Xilinx website) comes with the ZC706 (which uses the XC7Z045).

    The part number of the board on the Xilinx website (which comes with the ZC706) is AES-ZSDR3-ADI-G, while the one with the Zedboard is AES-ZSDR2-ADI-G.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • avnrdf
    0 avnrdf over 7 years ago

    It looks like they are different kits to begin with.

     

    The 'SDR II' uses the Zedboard (XC7Z020), but the the 'SDRIII' (or the Xilinx website) comes with the ZC706 (which uses the XC7Z045).

    The part number of the board on the Xilinx website (which comes with the ZC706) is AES-ZSDR3-ADI-G, while the one with the Zedboard is AES-ZSDR2-ADI-G.