Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard - Setting up multiple interrupts I2C0 and I2C1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 352 subscribers
  • Views 600 views
  • Users 0 members are here
Related

Zedboard - Setting up multiple interrupts I2C0 and I2C1

devinatkin
devinatkin over 6 years ago

Hello,

I've been trying to no avail to make use of both the I2C buses available on the Zedboard. I only have 2 devices, but they're connected to different external pins and given I have 2 busses I see no reason to make them share the lines.I've been working on a design and successfully implemented the first device. When I went to add the second Bus on the Zedboard output; however, when I enable the second bus the first device stops working and gets hung not receiving interrupts. This is kind of annoying and I can't find a solution so I'm moving on for now and setting them both up on the same bus, but I'm hoping someone can direct me towards a tutorial on how to make use of both the busses,

 

 

This was my initial I2C code from when I only had one bus enabled (It's based heavily on the example https://github.com/Xilinx/embeddedsw/blob/master/XilinxProcessorIPLib/drivers/iicps/examples/xiicps_intr_master_example.… )

int SetupIIC(){

 

 

XIicPs_Config *Config;

int Status;

 

 

    print("DAC IIC TEST\n\r");

 

 

Config = XIicPs_LookupConfig(XPAR_XIICPS_0_DEVICE_ID);

if (NULL == Config) {

return XST_FAILURE;

}

print("IIC Lookup Config Done \n\r");

 

 

Status = XIicPs_CfgInitialize(&Iic, Config, Config->BaseAddress);

if (Status != XST_SUCCESS) {

return XST_FAILURE;

}

print("IIC Cfg Initialize Done\n\r");

/*

* Perform a self-test to ensure that the hardware was built correctly.

*/

Status = XIicPs_SelfTest(&Iic);

if (Status != XST_SUCCESS) {

return XST_FAILURE;

}

print("IIC Self Test Done\n\r");

 

 

Status = SetupInterruptSystem(&Iic);

if (Status != XST_SUCCESS) {

return XST_FAILURE;

}

print("IIC Interrupts Setup\n\r");

 

 

XIicPs_SetStatusHandler(&Iic, (void *) &Iic, Handler);

 

 

print("IIC Status Handler Setup\n\r");

 

 

XIicPs_SetSClk(&Iic, IIC_SCLK_RATE);

 

 

Status = XIicPs_SetOptions(&Iic, XIICPS_7_BIT_ADDR_OPTION || XIICPS_REP_START_OPTION);

if (Status != XST_SUCCESS) {

return XST_FAILURE;

}

print("IIC 7 BIT Address Mode, repeated start\n\r");

 

 

 

 

print("IIC Setup Complete\n\r");

return XST_SUCCESS;

}

 

void Handler(void *CallBackRef, u32 Event)

{

/*

* All of the data transfer has been finished.

*/

if (0 != (Event & XIICPS_EVENT_COMPLETE_RECV)){

RecvComplete = TRUE;

} else if (0 != (Event & XIICPS_EVENT_COMPLETE_SEND)) {

SendComplete = TRUE;

 

 

} else if (0 != (Event & XIICPS_EVENT_NACK)) {

TotalNack++;

} else if (0 == (Event & XIICPS_EVENT_SLAVE_RDY)){

/*

* If it is other interrupt but not slave ready interrupt, it is

* an error.

* Data was received with an error.

*/

TotalErrorCount++;

}

}

 

 

 

static int SetupInterruptSystem(XIicPs *IicPsPtr)

 

 

{

int Status;

XScuGic_Config *IntcConfig; /* Instance of the interrupt controller */

 

 

Xil_ExceptionInit();

 

 

/*

* Initialize the interrupt controller driver so that it is ready to

* use.

*/

IntcConfig = XScuGic_LookupConfig(INTC_DEVICE_ID);

if (NULL == IntcConfig) {

return XST_FAILURE;

}

 

 

Status = XScuGic_CfgInitialize(&InterruptController, IntcConfig,

IntcConfig->CpuBaseAddress);

if (Status != XST_SUCCESS) {

return XST_FAILURE;

}

 

 

 

 

/*

* Connect the interrupt controller interrupt handler to the hardware

* interrupt handling logic in the processor.

*/

Xil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_IRQ_INT,

(Xil_ExceptionHandler)XScuGic_InterruptHandler,

&InterruptController);

 

 

/*

* Connect the device driver handler that will be called when an

* interrupt for the device occurs, the handler defined above performs

* the specific interrupt processing for the device.

*/

Status = XScuGic_Connect(&InterruptController, IIC_INT_VEC_ID,

(Xil_InterruptHandler)XIicPs_MasterInterruptHandler,

(void *)IicPsPtr);

if (Status != XST_SUCCESS) {

return Status;

}

 

 

/*

* Enable the interrupt for the Iic device.

*/

XScuGic_Enable(&InterruptController, IIC_INT_VEC_ID);

 

 

 

 

/*

* Enable interrupts in the Processor.

*/

Xil_ExceptionEnable();

 

 

return XST_SUCCESS;

}

 

This is what I ended at when trying to use multiple buses

/*****************************************************************************/

/**

*

* This function is the handler which performs processing to handle data events

* from the IIC.  It is called from an interrupt context such that the amount

* of processing performed should be minimized.

*

* This handler provides an example of how to handle data for the IIC and

* is application specific.

*

* @param CallBackRef contains a callback reference from the driver, in

* this case it is the instance pointer for the IIC driver.

* @param Event contains the specific kind of event that has occurred.

*

* @return None.

*

* @note None.

*

*******************************************************************************/

void AD5391_Handler(void *CallBackRef, u32 Event)

{

/*

* All of the data transfer has been finished.

*/

if (0 != (Event & XIICPS_EVENT_COMPLETE_RECV)){

AD5391_RecvComplete = TRUE;

} else if (0 != (Event & XIICPS_EVENT_COMPLETE_SEND)) {

AD5391_SendComplete = TRUE;

 

 

} else if (0 != (Event & XIICPS_EVENT_NACK)) {

AD5391_TotalNack++;

} else if (0 == (Event & XIICPS_EVENT_SLAVE_RDY)){

/*

* If it is other interrupt but not slave ready interrupt, it is

* an error.

* Data was received with an error.

*/

AD5391_TotalErrorCount++;

}

}

 

 

void HDMI_Handler(void *CallBackRef, u32 Event)

{

/*

* All of the data transfer has been finished.

*/

if (0 != (Event & XIICPS_EVENT_COMPLETE_RECV)){

HDMI_RecvComplete = TRUE;

} else if (0 != (Event & XIICPS_EVENT_COMPLETE_SEND)) {

HDMI_SendComplete = TRUE;

 

 

} else if (0 != (Event & XIICPS_EVENT_NACK)) {

HDMI_TotalNack++;

} else if (0 == (Event & XIICPS_EVENT_SLAVE_RDY)){

/*

* If it is other interrupt but not slave ready interrupt, it is

* an error.

* Data was received with an error.

*/

HDMI_TotalErrorCount++;

}

}

 

 

/******************************************************************************/

/**

*

* This function setups the interrupt system such that interrupts can occur

* for the IIC.  This function is application specific since the actual

* system may or may not have an interrupt controller.  The IIC could be

* directly connected to a processor without an interrupt controller.  The

* user should modify this function to fit the application.

*

* @param IicPsPtr contains a pointer to the instance of the Iic

* which is going to be connected to the interrupt controller.

*

* @return XST_SUCCESS if successful, otherwise XST_FAILURE.

*

* @note None.

*

*******************************************************************************/

static int SetupInterruptSystem(XIicPs *IicPsPtr, XIicPs *IicPsPtr1)

 

 

{

int Status;

XScuGic_Config *IntcConfig; /* Instance of the interrupt controller */

 

 

 

 

 

 

 

 

/*

* Initialize the interrupt controller driver so that it is ready to

* use.

*/

IntcConfig = XScuGic_LookupConfig(INTC_DEVICE_ID);

if (NULL == IntcConfig) {

return XST_FAILURE;

}

 

 

Status = XScuGic_CfgInitialize(&InterruptController, IntcConfig,

IntcConfig->CpuBaseAddress);

if (Status != XST_SUCCESS) {

return XST_FAILURE;

}

 

 

Status = XScuGic_SelfTest(&InterruptController);

if (Status != XST_SUCCESS) {

return XST_FAILURE;

}

 

 

/*

* Connect the interrupt controller interrupt handler to the hardware

* interrupt handling logic in the processor.

*/

Xil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_IRQ_INT,

(Xil_ExceptionHandler)XScuGic_InterruptHandler,

&InterruptController);

 

 

 

 

/*

* Enable non-critical exceptions.

*/

Xil_ExceptionEnable();

 

 

/*

* Connect the device driver handler that will be called when an

* interrupt for the device occurs, the handler defined above performs

* the specific interrupt processing for the device.

*/

Status = XScuGic_Connect(&InterruptController, IIC_INT_VEC_ID_AD5391,

(Xil_InterruptHandler)XIicPs_MasterInterruptHandler,

(void *)IicPsPtr);

if (Status != XST_SUCCESS) {

return Status;

}

 

 

XScuGic_Enable(&InterruptController, IIC_INT_VEC_ID_AD5391);

 

 

//XScuGic_SetPriorityTriggerType(&InterruptController, IIC_INT_VEC_ID_AD5391, 0XA0 , 0x3) ;

 

 

Status = XScuGic_Connect(&InterruptController, IIC_INT_VEC_ID_HDMI,

(Xil_InterruptHandler)XIicPs_MasterInterruptHandler,

(void *)IicPsPtr1);

 

 

if (Status != XST_SUCCESS) {

return Status;

}

 

 

XScuGic_Enable(&InterruptController, IIC_INT_VEC_ID_HDMI);

 

 

//XScuGic_SetPriorityTriggerType(&InterruptController, IIC_INT_VEC_ID_HDMI, 0XA8 , 0x3) ;

 

 

 

 

 

 

 

 

return XST_SUCCESS;

}

 

Any advice or directions to an appropriate tutorial would be much appreciated.