Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General USB 3.0 configuration Ultrazed EG
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 373 subscribers
  • Views 1305 views
  • Users 0 members are here
Related

USB 3.0 configuration Ultrazed EG

brignon
brignon over 7 years ago

Hi

 

I have configured my ultrazed under linux. When I plug USB drive to the Ultrazed USB3 plug, USB 2.0 devices are recognized properly, but USB 3.0 are not recognized and not visible.

When I connect the same USB3.0 devices to my linux Laptot, these devices are seen and recognized, means there is no issue on these devices.

 

In Vivado, I have enabled USB0 and selected USB3.0 / GT Lane0.

I have configured Linux using Petaliux and the following are enabled in the kernel:

Device Drivers------>

    USB support

        <*> xHCI HCD (USB 3.0) support

        <*> USB Mass Storage support

        <*> DesignWare USB3 DRD Core Support

        DWC3 Mode Selection (Dual Role mode)  --->

            (X) Dual Role mode

I purchased an adaptor USB3.0 in the market to plug the USB drives to the USB 3,0 plug of the Ultrazed carrier.

 

Is it anything specific to configure to have USB 3.0 devices working with the Ultrazed? Do we need to purchase a specific adapter (as I saw a recommandation for the ZC102 board)?

 

Thanks you in advance for your feedback

Best regards

Regis

  • Sign in to reply
  • Cancel

Top Replies

  • 100padudle
    100padudle over 6 years ago in reply to 100padudle +1
    I looked at the Petalinux settings and I think they have removed the device driver menu from 2019.1. I did not find anywhere to enable USB 3.0.
Parents
  • 100padudle
    0 100padudle over 6 years ago

    Hello Regis,

     

    I am trying to do exactly the same thing using the Ultrazed on the IO Carrier Card.  Did you ever determine if it is really possible and how?

     

    As an aside, I found that the SATA port works perfectly, as is, out of the box under linux.  Still, around the lab, a USB drive is much more convenient than a SATA SSD so I would love to get this working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to 100padudle

    I wonder if the signals for USB 3,0 are supported through the carrier board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100padudle
    0 100padudle over 6 years ago in reply to clem57

    Yes, the GTR signals are routed to the USB 3.0 connector on the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100padudle
    0 100padudle over 6 years ago in reply to 100padudle

    I looked at the Petalinux settings and I think they have removed the device driver menu from 2019.1.  I did not find anywhere to enable USB 3.0.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100padudle
    0 100padudle over 6 years ago in reply to 100padudle

    I looked at the Petalinux settings and I think they have removed the device driver menu from 2019.1.  I did not find anywhere to enable USB 3.0.