Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General UltraZed-EG SOM and IO carrier clock configuration
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 371 subscribers
  • Views 554 views
  • Users 0 members are here
  • ZedBoard General Questions
  • Zedboard Hardware Design
  • Ultrazed Hardware Design
Related

UltraZed-EG SOM and IO carrier clock configuration

youngk
youngk over 7 years ago

Hi,

I am testing UltraZed-EG SOM and IO carrier. But I couldn't get PL-SYSCLK (300MHz) working. I put jumper setting to default mode as following;

 

J1 and J2 placed on pins 1-2 and JP1 is not installed.

 

I put down simple VHDL test code and xdc file below. Please review and help me out.

Thanks,

Young

-------------------------------------------------------------------------------------------------------------------------------------------------------

entity test is

port (

          sysclk_p : in std_logic;

          sysclk_n : in std_logic;

          tp_1 : out std_logic;    --

--leds

         pl_led1 : out std_logic;    --

         pl_led2 : out std_logic    --

        );

end test;

architecture structure of test is

 

------*** signal declaration ***

signal sysclk : std_logic := '0';-- 

signal cnt: std_logic_vector(15 downto 0) := (others => '0');--

 

--#######################################################################################

begin

--=====================================================================

--Test signals

--=====================================================================

pl_led1 <= cnt(15);

pl_led2 <= '1';

tp_1 <= cnt(10);

--=====================================================================

--components instantiation

--=====================================================================

IBUFDS_1 : IBUFDS

generic map (

DQS_BIAS => "FALSE" -- (FALSE, TRUE)

)

port map (

O => sysclk, -- 1-bit output: Buffer output

I => sysclk_p, -- 1-bit input: Diff_p buffer input (connect directly to top-level port)

IB => sysclk_n -- 1-bit input: Diff_n buffer input (connect directly to top-level port)

);

 

process (sysclk)

begin

     if rising_edge(sysclk) then

          cnt <= cnt + 1;

     end if;

end process;

end structure;

--------------------------------------------------------------------------------------------------------------------------------------------------

test.xdc

----------------------------------------------------------------------------------------------------------------------------------------------------

set_property IOSTANDARD LVCMOS18 [get_ports pl_led1]

set_property IOSTANDARD LVCMOS18 [get_ports pl_led2]

 

 

set_property IOSTANDARD LVDS [get_ports sysclk_p]

set_property IOSTANDARD LVDS [get_ports sysclk_n]

 

 

set_property IOSTANDARD LVCMOS18 [get_ports tp_1]

 

 

#

set_property PACKAGE_PIN R7 [get_ports pl_led1]

set_property PACKAGE_PIN T5 [get_ports pl_led2]

 

 

 

 

set_property PACKAGE_PIN N4 [get_ports sysclk_p]

set_property PACKAGE_PIN N3 [get_ports sysclk_n]

 

 

set_property PACKAGE_PIN E2 [get_ports tp_1]

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi there,

     

    You really should be using that clock to feed into a MMCM or PLL.  You should not be using the clock directly.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi there,

     

    You really should be using that clock to feed into a MMCM or PLL.  You should not be using the clock directly.

     

    --Dan