Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Good quality DC Plug?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 371 subscribers
  • Views 579 views
  • Users 0 members are here
Related

Good quality DC Plug?

gizmo1990
gizmo1990 over 6 years ago

Can anyone recommend a 'good' quality DC plug? By good I mean good quality solid plastic shafts with well threaded and secure metal connectors/pins?

 

I want to avoid the poorly made ones which easily 'pull apart' when you pull them out because of the thin plastics used and poor threading.

 

I'd happily pay a little more to get a well made, secure barrel plug. However, sometimes paying more doesn't equate to better, so I'd like to know for sure if I'm actually getting quality for my money! There's so many barrel plugs on uk Farnell that I'm none to sure which to go for? The plug I'm after is an outer 5.5mm and inner 2.5mm.

 

Any advice greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +1 suggested
    There are only 10 the right size on Farnell, there is no point buying a Switchcraft locking one unless the mating part is the same type, so that leaves a choice between the Cliff FC6814775 at £2.39 and…
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    There are only 10 the right size on Farnell, there is no point buying a Switchcraft locking one unless the mating part is the same type, so that leaves a choice between the Cliff FC6814775 at £2.39 and the Switchcraft 765H at £3.77.

     

    Since I have never had one fail I would buy the cheap one.

    (that is I've never had one I fitted fail, I have replaced one or two from equipment, but usually because the cable failed and the plug was molded on.)

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 6 years ago

    There are only 10 the right size on Farnell, there is no point buying a Switchcraft locking one unless the mating part is the same type, so that leaves a choice between the Cliff FC6814775 at £2.39 and the Switchcraft 765H at £3.77.

     

    Since I have never had one fail I would buy the cheap one.

    (that is I've never had one I fitted fail, I have replaced one or two from equipment, but usually because the cable failed and the plug was molded on.)

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer