Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Need help with c64 psu
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 4 answers
  • Subscribers 375 subscribers
  • Views 987 views
  • Users 0 members are here
Related

Need help with c64 psu

wenmar
wenmar over 5 years ago

I know I need a 9vac for part of this but I only have a 110 to 15vdc brick is there a way to transform to 9vac, or can i trick with 9vdc and a 555 timer so the board thinks it is ac?

 

Any help would be appreciated!  Thank you in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 5 years ago in reply to ldeevans +1 suggested
    This is not always true. You need to be familiar with the circuit diagram for the equipment you're using to know for sure. Some pieces of equipment NEED a 9V AC supply as they use the AC to generate a…
  • baldengineer
    baldengineer over 5 years ago in reply to ldeevans +1 suggested
    This is not the case in the C64. The 9VAC supply is needed to generate a higher voltage necessary for the 12V rail, which drives the SID (sound) chip. The on-board power supply uses a capacitor voltage…
  • baldengineer
    baldengineer over 5 years ago in reply to wenmar +1 suggested
    No, you cannot bypass. The 9VAC supply is needed to generate a higher voltage necessary for the 12V rail, which drives the SID (sound) chip. The on-board power supply uses a capacitor voltage doubler to…
Parents
  • wenmar
    0 wenmar over 5 years ago

    Thank you!! Think i will try the bypass.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • baldengineer
    0 baldengineer over 5 years ago in reply to wenmar

    No, you cannot bypass.

     

    The 9VAC supply is needed to generate a higher voltage necessary for the 12V rail, which drives the SID (sound) chip. The on-board power supply uses a capacitor voltage doubler to step the 9 VAC to 18 volts. A DC supply will not work.

     

    It is also feed directly to the cassette drive to power the motors. The C64 needs a 9-12 VAC supply to operate correctly.

     

    You need to use a 120 to 9 V AC transformer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • baldengineer
    0 baldengineer over 5 years ago in reply to wenmar

    No, you cannot bypass.

     

    The 9VAC supply is needed to generate a higher voltage necessary for the 12V rail, which drives the SID (sound) chip. The on-board power supply uses a capacitor voltage doubler to step the 9 VAC to 18 volts. A DC supply will not work.

     

    It is also feed directly to the cassette drive to power the motors. The C64 needs a 9-12 VAC supply to operate correctly.

     

    You need to use a 120 to 9 V AC transformer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer