Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General ZedBoard (rev. D) not detected by Vivado
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 372 subscribers
  • Views 3363 views
  • Users 0 members are here
  • zedboard
  • vivado
Related

ZedBoard (rev. D) not detected by Vivado

dpdani
dpdani over 4 years ago

Hello,

I'm having trouble connecting my ZedBoard (rev. D) to Vivado.

It was already flashed, and I can see U-Boot/etc output over Tera Term, so I don't think there's a cable issue here.
I have downloaded the Cypress driver and the USB is managed by the correct driver:
image

But Vivado for some reason doesn't see it at all:

image

As far as I understand, the cable drivers in the Vivado distribution were installed correctly:

INFO: InstallPath="C:\Xilinx\Vivado\2021.2\data\xicom\cable_drivers\nt64\"
windrvr6 is not installed (this is expected for Windows 10 and later)
INFO: Installing Windows 10 pcusb driver...
Microsoft PnP Utility

Processing inf : xpcwinusb.inf
Driver package added successfully.
Published name : oem1.inf


Total attempted: 1
Number successfully imported: 1

INFO: INF file C:\Xilinx\Vivado\2021.2\data\xicom\cable_drivers\nt64\dlc10_win10\xpcwinusb.inf was successfully installed for driver.
INFO: Running digilent installer...

<<<<< Digilent Adept Runtime Setup >>>>>
Installer version: 1.5.8 release: 2018/06/22
Digilent Software Path: C:\Program Files (x86)\Digilent

Your system is up-to-date with the components of this installer.
INFO: Running SmartLynq installer...
INFO: SmartLynq installed successfully

My system info, in case it's relevant:
Processor Intel(R) Core(TM) i7-10750H CPU @ 2.60GHz 2.59 GHz
Installed RAM 16.0 GB (15.8 GB usable)
System type 64-bit operating system, x64-based processor
Edition Windows 11 Home
Version 21H2
Installed on ‎23/‎12/‎2021
OS build 22000.556
Experience Windows Feature Experience Pack 1000.22000.556.0

Any help would be greatly appreciated Pray

  • Sign in to reply
  • Cancel
Parents
  • dpdani
    dpdani over 4 years ago

    One additional note: my system doesn't have a USB port, so I'm connecting the board over a USB-C hub. Would that change anything?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bhfletcher
    bhfletcher over 4 years ago in reply to dpdani

    I have connected via JTAG to my boards using USB hubs before in Windows successfully. I've also seen with a Linux VM where that definitely did NOT work.

    I suggest you take a step back and do something simpler -- try a very simple hardware platform in Vivado, then export to Vitis and see if you can run Hello World. Note that the default baud rate for bare metal apps is 115200.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dpdani
    dpdani over 4 years ago in reply to bhfletcher

    Hello, thanks for the advice, but unfortunately it still didn't work.

    I've tried to implement this example project: https://digilent.com/reference/programmable-logic/guides/getting-started-with-ipi
    Once I try to run the project (the last step in the tutorial), Vitis comes up with this error:

    Error while launching program: 
    Could not find ARM device on the board for connection 'Local'.
    Check if the target is in:
    1. Split JTAG - No operations are possible with ARM DAP.
    2. Non JTAG bootmode - Bootrom may need time to enable DAP.
    Please try again.


    Troubleshooting hints:
    1. Check whether board is connected to system properly.
    2. In case of zynq board, check whether Digilent/Xilinx cable switch settings are correct.
    3. If you are using Xilinx Platform Cable USB, ensure that status LED is green.
    Could not find ARM device on the board for connection 'Local'.

    Also, the Vivado Hardware Manager still doesn't show any targets, as in the picture above.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dpdani
    dpdani over 4 years ago in reply to bhfletcher

    Hello, thanks for the advice, but unfortunately it still didn't work.

    I've tried to implement this example project: https://digilent.com/reference/programmable-logic/guides/getting-started-with-ipi
    Once I try to run the project (the last step in the tutorial), Vitis comes up with this error:

    Error while launching program: 
    Could not find ARM device on the board for connection 'Local'.
    Check if the target is in:
    1. Split JTAG - No operations are possible with ARM DAP.
    2. Non JTAG bootmode - Bootrom may need time to enable DAP.
    Please try again.


    Troubleshooting hints:
    1. Check whether board is connected to system properly.
    2. In case of zynq board, check whether Digilent/Xilinx cable switch settings are correct.
    3. If you are using Xilinx Platform Cable USB, ensure that status LED is green.
    Could not find ARM device on the board for connection 'Local'.

    Also, the Vivado Hardware Manager still doesn't show any targets, as in the picture above.