• Products and Partners
    Products and Partners
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
Avnet Boards Forums
  • Products and Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design Maaxboard not detecting HAT
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 581 views
  • Users 0 members are here
  • yocto image build
  • maaxboard
  • linux
Related

Maaxboard not detecting HAT

vinayingle
vinayingle over 3 years ago

I am trying to connect a raspberry pi compatible hat to maaxboard but there is not device file being created in the maaxboard yocto image. I have tested the uarts on the maaxboard and they seem to be working fine. I am lost on how to proceed next.

  • Sign in to reply
  • Cancel
  • tjaekel
    0 tjaekel over 3 years ago

    Assuming you are using a MaaXBoard (not MaaXBoard-RT, instead the "i.MX 8M MPU" board, but for both boards a similar response from me):
    How do you know that the HAT is now working?

    If a Raspberry Pi HAT (which one?) is plugged onto the header - how do you know it does not work?

    If your FW flashed and running would not use any pins on extension header (and therefore not anything on HAT) - nothing will happen
    if you just plug in the HAT board.

    You need a FW which would make use of it.
    The HW extension added does not install "automatically" the SW/FW for it.

    The fact, that "a" HAT is "pin-compatible" (which one? so many different HATs out there) does not mean yet anything.
    YOUR FW (project) has to use the HAT, configure the pins on extension header and use those.

    i think: if a HAT is compatible HW-wise with MaaXBoard (same pin functions and features), it should work if your FW configures pins on the extension header accordingly
    with the right functions. But w/o a FW using the HAT - why the HAT should not be detected when the FW "was told" there is now a HAT.

    It depends on the FW your are running
    (not using HAT - nothing happens).
    To plug in a HW extension does not do anything, esp. it does not generate a file in your IDE. (how?)