• Products and Partners
    Products and Partners
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
Avnet Boards Forums
  • Products and Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design MaaXBoard-RT: SPI bus with TWO SPI_CSx - solution
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 511 views
  • Users 0 members are here
  • gpio
  • MaaXBoard-RT
  • SPI_CS
  • spi
  • spi master
Related

MaaXBoard-RT: SPI bus with TWO SPI_CSx - solution

tjaekel
tjaekel over 3 years ago

The J1 pin table (see picture below) shows:
there is SPI_CS0 (fine, works, in "HW mode"), and SPI_CS1 (not possible in "HW mode" - how to use?).

I need a SPI bus with TWO SPI_CSx signals, so: SPI_CS0 and SPI_CS1 (as mentioned in pin table).

BTW:
I guess, there is just one SPI bus possible: I do not see any other pins possible to be used as SPI (only LPSPI4).

Based on the FW (SDK examples):
you can let generate SPI_CS0 (LPSPI_CS0) in "HW mode": this signal is generated when the SPI DMA kicks off and de-asserted when finished (automatically).
All fine.

But if I want to use a second CS signal (this SPI_CS1), for/at the same SPI bus (LPSPI4):
it is not possible:

  • to configure and use TWO SPI_CSx signals on the same SPI bus (not possible in driver code)
  • to use SPI_CS1 as any HW SPI CS signal:
    all the other pin_mux settings for PCS1...PCS3 crash, no way to let drive SPI_CS1 as a "HW mode" signal

Solution:

You have to change to generate the SPI_CSx signals in "SW mode".
It means:
You configure as GPIO Outputs and YOU drive both signals (now also SPI_CS0) by setting it low or high (for/during the SPI transaction).
It works.
But now both SPI_CSx signals must be handled in "SW mode". The "HW mode" (where SPI_CS0 is generated by DMA start and end),
is not usable anymore, it must be handled as a GPIO output as well.
It works.

You can see the implementation here:

tjaekel/MaaXBoard-RT_SPIder: MaaXBoard-RT SPIder framework (github.com)

The MaaXBoard-RT pin assignment table (for signals on J1):

MaaXBoard-RT J1