• Products and Partners
    Products and Partners
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
Avnet Boards Forums
  • Products and Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design MaaxBoard-RT: QSPI Master with "FastGPIO" - for you
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 466 views
  • Users 0 members are here
  • GPIO speed
  • qspi
  • gpio
  • MaaXBoard-RT
  • Maaxboard RT
  • Fast GPIO
Related

MaaxBoard-RT: QSPI Master with "FastGPIO" - for you

tjaekel
tjaekel over 3 years ago

I need a QSPI Master, with 40 MHz.
FLEXSPI (as QSPI) is not possible: two signals are missing on the extension headers.

So, I have implemented QSPI via "FastGPIO": it works:
41 MHz QSPI SCLK (potentially up to 60 MHz possible).

It is part now of my main project:
tjaekel/MaaXBoard-RT_SPIder: MaaXBoard-RT SPIder framework (github.com)

If you want to know "how I have implemented"...
See the file "pin_mux.c" where the GPIO pins are configured.
And see the file "QSPI_sw.c" (plus *.h) how I toggle the GPIO pins.

  /* configure LPSPI2 as FastGPIO pins - for SW QSPI master */
  IOMUXC_GPR->GPR43 = 0x00000F84;				/* select FastGPIO, CM7_GPIO3, bits 23, 24, 25, 26, 27, 18 */

  GPIO_PinInit(CM7_GPIO3, 23U, &USER_GPIO_config);
  GPIO_PinInit(CM7_GPIO3, 24U, &USER_GPIO_config);
  GPIO_PinInit(CM7_GPIO3, 25U, &USER_GPIO_config);
  GPIO_PinInit(CM7_GPIO3, 26U, &USER_GPIO_config);
  GPIO_PinInit(CM7_GPIO3, 27U, &USER_GPIO_config);
  GPIO_PinInit(CM7_GPIO3, 18U, &USER_GPIO_config);

  IOMUXC_SetPinMux(
		  IOMUXC_GPIO_AD_24_GPIO_MUX3_IO23,     /* configured as GPIO - SCLK */
      0x0U);

  IOMUXC_SetPinConfig(
		  IOMUXC_GPIO_AD_24_GPIO_MUX3_IO23,
	  0x03U);

  IOMUXC_SetPinMux(
		  IOMUXC_GPIO_AD_25_GPIO_MUX3_IO24,     /* configured as GPIO - PCS0*/
      0x0U);

  IOMUXC_SetPinConfig(
		  IOMUXC_GPIO_AD_25_GPIO_MUX3_IO24,
	  0x03U);

  IOMUXC_SetPinMux(
		  IOMUXC_GPIO_AD_26_GPIO_MUX3_IO25,     /* configured as GPIO - D0 */
      0x0U);

  IOMUXC_SetPinConfig(
		  IOMUXC_GPIO_AD_26_GPIO_MUX3_IO25,
	  0x03U);

  IOMUXC_SetPinMux(
		  IOMUXC_GPIO_AD_27_GPIO_MUX3_IO26,     /* configured as GPIO - D1 */
      0x0U);

  IOMUXC_SetPinConfig(
		  IOMUXC_GPIO_AD_27_GPIO_MUX3_IO26,
	  0x03U);

  IOMUXC_SetPinMux(
		  IOMUXC_GPIO_AD_28_GPIO_MUX3_IO27,     /* configured as GPIO - D2 */
      0x0U);

  IOMUXC_SetPinConfig(
		  IOMUXC_GPIO_AD_28_GPIO_MUX3_IO27,
  	  0x03U);

  IOMUXC_SetPinMux(
		  IOMUXC_GPIO_AD_19_GPIO_MUX3_IO18,     /* configured as GPIO - D3 */
      0x0U);

  IOMUXC_SetPinConfig(
		  IOMUXC_GPIO_AD_19_GPIO_MUX3_IO18,
	  0x03U);
	  

/*
 * QSPI_sw.c
 *
 *  Created on: Sep 11, 2023
 *      Author: tjaekel
 */

/* QSPI in SW GPIO mode (as FastGPIO) */

#include <stdio.h>
#include <stdlib.h>
#include "fsl_gpio.h"

#include "QSPI_sw.h"

#include "MEMORY_attributes.h"

/* trimmed for 41 MHz, periodic SCLK
 * our scope has 500 MHz sampling rate, to 2ns error,
 * MCU runs with 1 GHz, assuming 2 cycles per __NOP() is also 2ns
 * It looks "perfect", the 'jitter' and inaccuracy comes from the scope!
 */

/* for SCLK low period */
#define NOP_DELAY 	__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP()

/* for SCLK high period */
#define NOP_DELAY2 	__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP()

/* last in loop high period */
#define NOP_DELAY2b __NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP()

/* last (2nd) delay on first byte, before entering loop */
#define NOP_DELAY3 	__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP();\
					__NOP()

uint8_t GPIO_QSPIbuffer[16] = {0xA5, 0x5A, 0x12, 0x21, 0x44, 0x88, 0x77, 0x42, 0x55, 0x66, 0x77, 0x88, 0x99, 0xAA, 0xBB, 0xCC};

void QSPI_Init(void)
{
	/* set PCS signal high, all other low */
	/* optional: we could have all signals except PCS as inputs (tri-stated) */
	CM7_GPIO3->DR_SET = (1 << QSPI_PCSbit);
	CM7_GPIO3->DR_CLEAR = (1 << QSPI_SCLKbit) | ( 1 << QSPI_D0bit) | (1 << QSPI_D1bit) | (1 << QSPI_D2bit) | (1 << QSPI_D3bit);
}

#pragma GCC push_options
#pragma GCC optimize ("O3")

ITCM_CM7 void QSPI_SendWrite(uint8_t *buf, size_t numBytes)
{
	uint8_t b;
	uint32_t w;

	__asm volatile ( "cpsid i" ::: "memory" );
	__asm volatile ( "dsb" );
	__asm volatile ( "isb" );

	/* Set Direction of QSPI D0..D3 as output */


	/* 2. Set initial D0..D1 - PCS still high, SCLK starting low */
	b = *buf++;
	/* TODO: we could handle 3 bits at once */
	w  = (b & 0x10) << (QSPI_D0bit - 4);
	w |= (b & 0x20) << (QSPI_D1bit - 5);
	w |= (b & 0x40) << (QSPI_D2bit - 6);
	w |= (b & 0x80) << (QSPI_D3bit - 7);

	w |= 1 << QSPI_PCSbit;
	CM7_GPIO3->DR = w;
	////__NOP();

	/* Set and keep PCS low */
	w &= ~(1 << QSPI_PCSbit);
	CM7_GPIO3->DR = w;

	NOP_DELAY;

	w |= 1 << QSPI_SCLKbit;
	CM7_GPIO3->DR = w;

	/* keep D0..D1 stable half a clock period on SCLK high */
	NOP_DELAY2;

	/* set SCLK low (falling edge, change to next 4bit Dx) */
	w  = (b & 0x01) << (QSPI_D0bit - 0);
	w |= (b & 0x02) << (QSPI_D1bit - 1);
	w |= (b & 0x04) << (QSPI_D2bit - 2);
	w |= (b & 0x08) << (QSPI_D3bit - 3);
	CM7_GPIO3->DR = w;

	/* wait half a clock period with SCLK low */
	NOP_DELAY;

	/* SCLK high */
	w |= 1 << QSPI_SCLKbit;
	CM7_GPIO3->DR = w;

	NOP_DELAY3;
	numBytes--;

	while (numBytes--)
	{
		b = *buf++;
		w  = (b & 0x10) << (QSPI_D0bit - 4);
		w |= (b & 0x20) << (QSPI_D1bit - 5);
		w |= (b & 0x40) << (QSPI_D2bit - 6);
		w |= (b & 0x80) << (QSPI_D3bit - 7);

		CM7_GPIO3->DR = w;

		NOP_DELAY;

		w |= 1 << QSPI_SCLKbit;
		CM7_GPIO3->DR = w;

		NOP_DELAY2;

		w  = (b & 0x01) << (QSPI_D0bit - 0);
		w |= (b & 0x02) << (QSPI_D1bit - 1);
		w |= (b & 0x04) << (QSPI_D2bit - 2);
		w |= (b & 0x08) << (QSPI_D3bit - 3);
		CM7_GPIO3->DR = w;

		NOP_DELAY;

		w |= 1 << QSPI_SCLKbit;
		CM7_GPIO3->DR = w;

		NOP_DELAY2b;
	}

	/* Set PCS high */
	w |= 1 << QSPI_PCSbit;
	CM7_GPIO3->DR = w;

	/* change D0..D1 direction to input (tri-state) */

	__asm volatile ( "cpsie i" ::: "memory" );
}

#pragma GCC pop_options

void QSPI_Test(void)
{
	size_t i;

	QSPI_Init();
	QSPI_SendWrite(GPIO_QSPIbuffer, 16);
}

/*
 * QSPI_sw.h
 *
 *  Created on: Sep 11, 2023
 *      Author: tjaekel
 */

#ifndef QSPI_SW_H_
#define QSPI_SW_H_

#define	QSPI_SCLKbit		23
#define QSPI_PCSbit			24
#define	QSPI_D0bit			25
#define	QSPI_D1bit			26
#define	QSPI_D2bit			27
#define	QSPI_D3bit			18

void QSPI_Test(void);

#endif /* QSPI_SW_H_ */