• Products and Partners
    Products and Partners
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
Avnet Boards Forums
  • Products and Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design MaaxBoard-RT: QSPI with FLEXIO2 - for you
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 530 views
  • Users 0 members are here
  • qspi
  • MaaXBoard-RT
  • SDK example
  • Maaxboard RT
  • spi master
Related

MaaxBoard-RT: QSPI with FLEXIO2 - for you

tjaekel
tjaekel over 3 years ago

I could implement the QSPI on the available header pins also via FLEXIO2 (instead of "FastGPIO").
It works (at least the QSPI write waveform looks correct).

The project is here:

tjaekel/MaaXBoard-RT_flexio_qspi_edma_cm7: QSPI with FLEXIO2 and EDMA (github.com)

Is uses FLEXIO2 pins and FLEXIO2 to generate the 4 bit parallel QSPI data lanes.

It works up to 30 MHz, 60 MHz might have a bit "strange" waveform.

Remark:

The project is still under development - I need to add QSPI read
(change the pin direction, but similar approach).

It has modified SDK drivers !!, e.g. "fsl_flexio_spi.c": I have 'hijacked' the FLEXIO SPI drivers for it
(see the macro "FLEXIO_QSPI" added).
I had to modify the shifter configuration, esp. the WIDTH and the TIMER for the SCLK signal,