• Products and Partners
    Products and Partners
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
Avnet Boards Forums
  • Products and Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design MaaxBoard-RT: HAT - SPI plus QSPI as HAT
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 715 views
  • Users 0 members are here
  • pins
  • qspi
  • gpio
  • MaaXBoard-RT
  • Maaxboard RT
  • SPI slave
  • DualSPIder
  • spi master
  • pinmux
  • maaxboard
  • Pin Mux
Related

MaaxBoard-RT: HAT - SPI plus QSPI as HAT

tjaekel
tjaekel over 3 years ago

FYI,

I am going to create a breakout board (HAT), a PCB, in order to have SPI and QSPI interfaces on headers for this MaaxBoard-RT board (using J1 and J15).
The board should have these "features":

  • "DualSPI":
    SPI2 is master (Tx only), SPI4 is slave (Rx only) (uni-directional use), using a "delayed" SCLK' signal (compensate "round trip delay")
    SPI4 slave (Rx) will not use a PCS (nCS) HW signal (SW based enable)
    main requirement to have SPI with "delay compensation" for external devices connected (2x on same SPI bus)
  • optional to use LPSPI2 as bi-directional master/slave
  • LPSPI1:
    optional: a full bi-directional master/slave (in addition to all other SPIs and QSPI)
  • EEPROM:
    Use I2C6 for an I2C flash device (persistent storage of SYSCFG, man pages, optional "plug-in" code, "device tree"... - like on Raspberry Pi)
  • LPUART2/SPDIF_IN and _OUT, I2C3:
    provide as header pins, e.g. for user UART, SPDIF
  • I2C5:
    optional I2C, but shared with onboard I2C DAC (and with 2K2 pull-up already on MaaxBoard-RT)
  • I2S Master:
    provide the PCM signals as Master Out for an external DAC (in addition to onboard DAC)
  • PDM:
    one stereo channel for external MICs (as addition/alternative to onboard MICs)
  • ACMP signals: keep the Analog Comparator signals available
  • QSPI on header as: SW GPIO or FLEXIO2 QSPI
    SW GPIO QSPI should pin-compatible with SPI interface (FLEXIO2 would not)
    my main requirement to have QSPI for an external device
  • QSPI as FLEXIO:
    a QSPI flash on HAT board (for testing, for additional code/data, in parallel with header, two nCS signals for onboard QSPI and header QSPI)
  • free pins used as GPIO
  • RESET signals as GPIO out, INT signals as GPIO in, for external device connected

Here is the PinMux Table (how I want to use the MaaxBoard-RT header pins):

MaaxBoard-RT HAT header pins (pinmux)

Figure 1: MaaxBoard-RT HAT header pins and pinmux functions

Schematics for it might follow...
You could use this table also as reference for the pins and what might be possible with those (pinmux).

  • Sign in to reply
  • Cancel
  • tjaekel
    tjaekel over 3 years ago

    Here now how I want to use the MaaxBoard-RT pins and wire:

    QSPI wiring

    Figure 2: MaaxBoard-RT QSPI HAT wiring

    Comments:

    I want to use a CPLD, e.g. as level shifter and to deal with the direction (WR vs. WR+RD), for the additional HW logic.

    When I use FLEXIO2 and it is a QSPI RD transaction: the FLEXIO2 must be reconfigured to do a RD (after the WR with the prefix),
    change the direction on FLEXIO2.
    If the F_nCSx signal is generated also by the FLEXIO2 - it will be de-asserted between WR + RD. Therefore, I want to force via GPIO signal F_AND
    to keep this F_nCSx signal low between WR + RD.
    Not sure if I can handle the F_nCSx signals in SW: I want to make sure that this signal is valid after FLEXIO2 starts, not too early with floating QSPI signals.

    Instead of using a bi-directional level shifter, I want to have the option to use uni-directional drivers, e.g. in a CPLD.
    The F_DIR signal should change the direction.

    The CPLD (and its logic) is optional.

    The QSPI headers will have a 3V3 pin, so that the level shifter logic (and F_DIR) can be part of a breakout unit ("in the cable").