Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design Using the Secure Non Volatile Storage (SNVS) on a Maaxboard. External power source needed.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 996 views
  • Users 0 members are here
Related

Using the Secure Non Volatile Storage (SNVS) on a Maaxboard. External power source needed.

tom-h
tom-h over 1 year ago

Hi All, 

I'm currently trying to use the Secure Non Volatile Storage (SNVS) on my Maaxboard. In the IMX8M technical specification (i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual) it states that:

"

Throughout the SNVS documentation whenever mention is
made of "always-on" logic, this assumes a version of SNVS that implements an
independent power domain for the LP section, and that the power for this section is
supplied by an uninterrupted power supply. The purpose for the independent power
domain is so that data can be retained and certain logic can remain functional even when
the main chip logic is powered down. But this is possible only if the LP domain remains
powered via an uninterrupted power supply when the main chip power domain is
powered off. Usually this uninterrupted power supply would be a battery, with possibly
some power management logic to power the LP section from main power (and perhaps

recharge the battery) when main power is on, and switch to battery power when the main
power is off. In versions of SNVS with an independent LP power domain the LP section
can be electrically isolated from the rest of the chip logic to ensure that its logic does not
get corrupted when the main chip is powered down

"

It doesn't appear that the maaxboard has a a battery. Has anyone tried to supply a battery or an additional power source to use the SVNS? Is this possible?

Any help with this would be greatly appreciated.

Thanks, 

Tom

  • Sign in to reply
  • Cancel

Top Replies

  • bidrohini
    bidrohini over 1 year ago +1
    You can use a small coin-cell battery (e.g., CR2032 or rechargeable LIR2032) connected to the identified SNVS LP power pin. https://www.theengineeringprojects.com/2021/05/cr2032-lithium-coin-library-for…
  • bidrohini
    bidrohini over 1 year ago

    You can use a small coin-cell battery (e.g., CR2032 or rechargeable LIR2032) connected to the identified SNVS LP power pin. https://www.theengineeringprojects.com/2021/05/cr2032-lithium-coin-library-for-proteus.html Include a diode to prevent backfeeding the main power to the battery and a resistor to limit charging current if using a rechargeable battery. Alternatively, you can use a supercapacitor or and external DC source.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • TheSanjanaSuresh
    TheSanjanaSuresh over 1 year ago in reply to bidrohini

    Does the MaaxBoard RT have an SNVS LP pin?