Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design LPADC Interrupt - Reading Constant 4095
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 358 subscribers
  • Views 821 views
  • Users 0 members are here
  • MaaXBoard-RT
  • SDK example
  • lpadc
Related

LPADC Interrupt - Reading Constant 4095

TheSanjanaSuresh
TheSanjanaSuresh over 1 year ago

Hello All,

I am currently trying to implement an LPADC interrupt-driven application on the MAAXBOARD RT. To get started. Specifically, I am attempting to read analog values from the following GPIO pins:

  • GPIO_AD_13
  • GPIO_AD_19
  • GPIO_AD_15

However, when I read the ADC values from these pins, I consistently receive a value of 4095. This occurs across all three pins.

Could you please provide some insight into what might be causing this issue? I suspect there might be a configuration problem or a misunderstanding on my part regarding the hardware or software setup for these specific GPIO pins on the MIMXRT1176DVMAA within the MAAXBOARD RT context.

Any guidance or suggestions on how to troubleshoot this constant reading of 4095 would be greatly appreciated. I am available to provide further details about my setup or the modifications I have made to the example code if needed.

Thank you for your time and assistance.

Regards,

Sanjana S

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 1 year ago +1
    Is there a pull-up resistor enabled on the input?
  • michaelkellett
    michaelkellett over 1 year ago in reply to TheSanjanaSuresh +1
    I had a quick look at the reference manual and the data sheet for the processor and found them to be very unclear. I think it is possible that the use of a Vref = 3.3V is not supported. Unfortunately…
Parents
  • dougw
    0 dougw over 1 year ago

    Is there a pull-up resistor enabled on the input?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • TheSanjanaSuresh
    0 TheSanjanaSuresh over 1 year ago in reply to dougw

    No, this is my configuration for GPIO_AD_16 (note: GPIO_AD_15 does not exist on this device):

    IOMUXC_SetPinConfig(

    IOMUXC_GPIO_AD_16_GPIO_MUX3_IO15,

    0x02U);

    This configuration, based on the default provided by the SDK examples, has a changed register value and is working correctly.

    However, I am encountering an issue with the reference voltage for the ADC. I am consistently getting 1.89V, but I need to set it to 3.3V.

    According to the datasheet of MIMXRT1176DVMAA:

    VDDA_ADC_1P8: 1.65V to1.95V

    VDDA_ADC_3P3: 3.0V to 3.6V

    ADC_VREFH: 1.0V to 1.89V

    It seems that when I use kLPADC_ReferenceVoltageAlt1, it correctly selects ADC_VREFH, resulting in the 1.89V reading. How can I configure the ADC to use a 3.3V reference voltage (likely VDDA_ADC_3P3)? I am getting 1.89V maxx even when I try other reference voltage configurations.

    Note: Remaing 

    • GPIO_AD_13
    • GPIO_AD_19 still I'm getting 4095 reanding

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 1 year ago in reply to TheSanjanaSuresh

    I had a quick look at the reference manual and the data sheet for the processor and found them to be very unclear. I think it is possible that the use of a Vref = 3.3V is not supported.

    Unfortunately the reference manual refers to Vssa which is not to be found in the data sheet.

    I think you will need to ask NXP tech support Slight frown

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 1 year ago in reply to TheSanjanaSuresh

    I had a quick look at the reference manual and the data sheet for the processor and found them to be very unclear. I think it is possible that the use of a Vref = 3.3V is not supported.

    Unfortunately the reference manual refers to Vssa which is not to be found in the data sheet.

    I think you will need to ask NXP tech support Slight frown

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • TheSanjanaSuresh
    0 TheSanjanaSuresh over 1 year ago in reply to michaelkellett

    Ok. Thank You!