Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MaaXBoard Hardware Design Does maaxboard have yocto support? Which branch is currently maintained?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 657 views
  • Users 0 members are here
  • yocto
  • maaxboard
Related

Does maaxboard have yocto support? Which branch is currently maintained?

moose_rivieh
moose_rivieh 11 months ago

Meta-maaxboard documentation lists the following branches as supported for the various maaxboard models

A meta-layer for MaaXBoard series boards

  • Yocto scarthgap(5.0) support : MaaXBoard-8ULP
  • Yocto nanbield(4.2) support : MaaXBoard-Osm93
  • Yocto Mickledore(4.2) support : MaaXBoard-8ULP
  • Yocto Langdale(4.1) support : MaaXBoard/MaaXBoard-Mini/MaaXBoard-Nano/MaaXBoard-8ULP
  • Yocto Kirkstone(4.0) support : MaaXBoard/MaaXBoard-Mini/MaaXBoard-Nano/MaaXBoard-8ULP

I have the maaxboard (AES-MC-SBC-IMX8M-G) and I was able to build both avnet-image-lite and avnet-image-full using Langdale branch with no issues. However, neither images boot and got the below kernel panic. Isn't this the correct branch? Is this board maintained or obsolete? I would expect these images to load out of the box. Below is the kernel log for both boots.

U-Boot SPL 2022.04-lf_v2022.04+g0dd7e59924d (Sep 26 2023 - 07:43:51 +0000)
power_bd71837_init
set buck8 to 1.2v for DDR4
DDRINFO: start DRAM init
DDRINFO: DRAM rate 2400MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1


U-Boot 2022.04-lf_v2022.04+g0dd7e59924d (Sep 26 2023 - 07:43:51 +0000)

CPU: i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)
CPU: Commercial temperature grade (0C to 95C) at 39C
Reset cause: POR
Model: Avnet MaaXBoard
DRAM: 2 GiB
Core: 56 devices, 18 uclasses, devicetree: separate
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial

BuildInfo:
- ATF fccc380

switch to partitions #0, OK
mmc0 is current device
flash target is MMC:0
Net:
Warning: ethernet@30be0000 (eth0) using random MAC address - f2:82:a4:34:51:79
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
858 bytes read in 1 ms (837.9 KiB/s)
32512512 bytes read in 1355 ms (22.9 MiB/s)
52629 bytes read in 4 ms (12.5 MiB/s)
Applying DT overlay => ext-gpio.dtbo
575 bytes read in 2 ms (280.3 KiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004301ffff
Remove /soc@0/bus@30800000/ethernet@30be0000:phy-reset-gpios

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 6.1.1+gd59104ae45c4 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 12.2.0, GNU ld (GNU Binutils) 2.39.0.20220819) #1 SMP PREEMPT Thu Sep 7 06:56:02 UTC 2023
[ 0.000000] Machine model: Avnet MaaXBoard
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000044000000, size 960 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbfbc1700-0xbfbc3fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s44520 r8192 d29208 u81920
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc0,115200 console=tty1 root=/dev/mmcblk0p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] Memory: 1041108K/2097152K available (19904K kernel code, 1606K rwdata, 6788K rodata, 3328K init, 645K bss, 73004K reserved, 983040K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 8.33MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns
[ 0.000000] sched_clock: 56 bits at 8MHz, resolution 120ns, wraps every 2199023255541ns
[ 0.000455] Console: colour dummy device 80x25
[ 0.000926] printk: console [tty1] enabled
[ 0.001005] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.66 BogoMIPS (lpj=33333)
[ 0.001033] pid_max: default: 32768 minimum: 301
[ 0.001108] LSM: Security Framework initializing
[ 0.001216] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.001245] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.002819] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.002843] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.002932] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.003122] rcu: Hierarchical SRCU implementation.
[ 0.003135] rcu: Max phase no-delay instances is 1000.
[ 0.004267] EFI services will not be available.
[ 0.004497] smp: Bringing up secondary CPUs ...
[ 0.004980] Detected VIPT I-cache on CPU1
[ 0.005062] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.005101] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.005617] Detected VIPT I-cache on CPU2
[ 0.005689] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.005712] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.006178] Detected VIPT I-cache on CPU3
[ 0.006254] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.006276] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.006336] smp: Brought up 1 node, 4 CPUs
[ 0.006427] SMP: Total of 4 processors activated.
[ 0.006441] CPU features: detected: 32-bit EL0 Support
[ 0.006452] CPU features: detected: 32-bit EL1 Support
[ 0.006465] CPU features: detected: CRC32 instructions
[ 0.006544] CPU: All CPU(s) started at EL2
[ 0.006573] alternatives: applying system-wide alternatives
[ 0.008641] devtmpfs: initialized
[ 0.016207] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.016273] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.045619] pinctrl core: initialized pinctrl subsystem
[ 0.047751] DMI not present or invalid.
[ 0.048407] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.049661] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.049903] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.050076] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.050129] audit: initializing netlink subsys (disabled)
[ 0.050277] audit: type=2000 audit(0.048:1): state=initialized audit_enabled=0 res=1
[ 0.050800] thermal_sys: Registered thermal governor 'step_wise'
[ 0.050805] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.050852] cpuidle: using governor menu
[ 0.051051] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.051147] ASID allocator initialised with 65536 entries
[ 0.052107] Serial: AMBA PL011 UART driver
[ 0.052183] imx mu driver is registered.
[ 0.052212] imx rpmsg driver is registered.
[ 0.059149] imx8mq-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.069192] KASLR disabled due to lack of seed
[ 0.089883] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.089906] HugeTLB: 16380 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.089922] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.089935] HugeTLB: 508 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.089950] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.089964] HugeTLB: 28 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.089979] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.089993] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.091786] ACPI: Interpreter disabled.
[ 0.092344] iommu: Default domain type: Translated
[ 0.092360] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.092697] SCSI subsystem initialized
[ 0.093040] usbcore: registered new interface driver usbfs
[ 0.093090] usbcore: registered new interface driver hub
[ 0.093131] usbcore: registered new device driver usb
[ 0.093969] mc: Linux media interface: v0.10
[ 0.094014] videodev: Linux video capture interface: v2.00
[ 0.094109] pps_core: LinuxPPS API ver. 1 registered
[ 0.094122] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.094151] PTP clock support registered
[ 0.094281] EDAC MC: Ver: 3.0.0
[ 0.095202] FPGA manager framework
[ 0.095292] Advanced Linux Sound Architecture Driver Initialized.
[ 0.095920] Bluetooth: Core ver 2.22
[ 0.095960] NET: Registered PF_BLUETOOTH protocol family
[ 0.095973] Bluetooth: HCI device and connection manager initialized
[ 0.095993] Bluetooth: HCI socket layer initialized
[ 0.096007] Bluetooth: L2CAP socket layer initialized
[ 0.096029] Bluetooth: SCO socket layer initialized
[ 0.096379] vgaarb: loaded
[ 0.096900] clocksource: Switched to clocksource arch_sys_counter
[ 0.097097] VFS: Disk quotas dquot_6.6.0
[ 0.097148] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.097339] pnp: PnP ACPI: disabled
[ 0.104644] NET: Registered PF_INET protocol family
[ 0.104854] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.106688] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.106760] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.106789] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.106934] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 0.107424] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.107533] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.107595] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.107753] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.108089] RPC: Registered named UNIX socket transport module.
[ 0.108106] RPC: Registered udp transport module.
[ 0.108117] RPC: Registered tcp transport module.
[ 0.108129] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.108993] PCI: CLS 0 bytes, default 64
[ 0.109713] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.110335] kvm [1]: IPA Size Limit: 40 bits
[ 0.111890] kvm [1]: vgic-v2@31020000
[ 0.111915] kvm [1]: GIC system register CPU interface enabled
[ 0.112012] kvm [1]: vgic interrupt IRQ9
[ 0.112114] kvm [1]: Hyp mode initialized successfully
[ 0.113311] Initialise system trusted keyrings
[ 0.113473] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.120572] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.121317] NFS: Registering the id_resolver key type
[ 0.121352] Key type id_resolver registered
[ 0.121365] Key type id_legacy registered
[ 0.121451] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.121468] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.121505] ntfs: driver 2.1.32 [Flags: R/W].
[ 0.121686] ntfs3: Max link count 4000
[ 0.121699] ntfs3: Enabled Linux POSIX ACLs support
[ 0.121710] ntfs3: Read-only LZX/Xpress compression included
[ 0.121797] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.122136] 9p: Installing v9fs 9p2000 file system support
[ 0.165029] Key type asymmetric registered
[ 0.165046] Asymmetric key parser 'x509' registered
[ 0.165100] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.165120] io scheduler mq-deadline registered
[ 0.165133] io scheduler kyber registered
[ 0.170332] EINJ: ACPI disabled.
[ 0.178065] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.178101] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.181323] mxs-dma 33000000.dma-apbh: initialized
[ 0.185727] SoC: i.MX8MQ revision 2.1
[ 0.185839] Config NOC for VPU and CPU
[ 0.186441] Bus freq driver module loaded
[ 0.191770] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.193881] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 18, base_baud = 1562500) is a IMX
[ 1.273807] printk: console [ttymxc0] enabled
[ 1.278819] 30a60000.serial: ttymxc3 at MMIO 0x30a60000 (irq = 19, base_baud = 5000000) is a IMX
[ 1.299657] loop: module loaded
[ 1.303846] of_reserved_mem_lookup() returned NULL
[ 1.308819] megasas: 07.719.03.00-rc1
[ 1.313821] imx ahci driver is registered.
[ 1.322713] tun: Universal TUN/TAP device driver, 1.6
[ 1.328471] thunder_xcv, ver 1.0
[ 1.331769] thunder_bgx, ver 1.0
[ 1.335046] nicpf, ver 1.0
[ 1.339450] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.346695] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.352072] hclge is initializing
[ 1.355414] e1000: Intel(R) PRO/1000 Network Driver
[ 1.360307] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.366106] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.371091] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.377068] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.382484] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.388101] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.394385] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.400459] sky2: driver version 1.30
[ 1.404614] usbcore: registered new interface driver r8152
[ 1.410368] VFIO - User Level meta-driver version: 0.3
[ 1.418179] usbcore: registered new interface driver uas
[ 1.423561] usbcore: registered new interface driver usb-storage
[ 1.429673] usbcore: registered new interface driver usbserial_generic
[ 1.436237] usbserial: USB Serial support registered for generic
[ 1.442294] usbcore: registered new interface driver ftdi_sio
[ 1.448075] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.455434] usbcore: registered new interface driver usb_serial_simple
[ 1.461996] usbserial: USB Serial support registered for carelink
[ 1.468127] usbserial: USB Serial support registered for zio
[ 1.473823] usbserial: USB Serial support registered for funsoft
[ 1.479862] usbserial: USB Serial support registered for flashloader
[ 1.486250] usbserial: USB Serial support registered for google
[ 1.492209] usbserial: USB Serial support registered for libtransistor
[ 1.498770] usbserial: USB Serial support registered for vivopay
[ 1.504809] usbserial: USB Serial support registered for moto_modem
[ 1.511109] usbserial: USB Serial support registered for motorola_tetra
[ 1.517756] usbserial: USB Serial support registered for nokia
[ 1.523622] usbserial: USB Serial support registered for novatel_gps
[ 1.530012] usbserial: USB Serial support registered for hp4x
[ 1.535790] usbserial: USB Serial support registered for suunto
[ 1.541743] usbserial: USB Serial support registered for siemens_mpi
[ 1.548144] usbcore: registered new interface driver usb_ehset_test
[ 1.556772] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 1.571160] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.577384] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 1.586546] i2c_dev: i2c /dev entries driver
[ 1.594998] Bluetooth: HCI UART driver ver 2.3
[ 1.599473] Bluetooth: HCI UART protocol H4 registered
[ 1.604629] Bluetooth: HCI UART protocol BCSP registered
[ 1.609979] Bluetooth: HCI UART protocol LL registered
[ 1.615136] Bluetooth: HCI UART protocol ATH3K registered
[ 1.620568] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.626933] Bluetooth: HCI UART protocol Broadcom registered
[ 1.632631] Bluetooth: HCI UART protocol QCA registered
[ 1.639285] sdhci: Secure Digital Host Controller Interface driver
[ 1.645495] sdhci: Copyright(c) Pierre Ossman
[ 1.650433] Synopsys Designware Multimedia Card Interface Driver
[ 1.656994] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.664847] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.671630] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.678602] usbcore: registered new interface driver usbhid
[ 1.684204] usbhid: USB HID core driver
[ 1.692129] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.697503] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 1.703388] NET: Registered PF_LLC protocol family
[ 1.711894] NET: Registered PF_INET6 protocol family
[ 1.719889] Segment Routing with IPv6
[ 1.723615] In-situ OAM (IOAM) with IPv6
[ 1.727615] NET: Registered PF_PACKET protocol family
[ 1.732735] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 1.747354] Bluetooth: RFCOMM TTY layer initialized
[ 1.752262] Bluetooth: RFCOMM socket layer initialized
[ 1.757439] Bluetooth: RFCOMM ver 1.11
[ 1.761224] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.766563] Bluetooth: BNEP filters: protocol multicast
[ 1.771822] Bluetooth: BNEP socket layer initialized
[ 1.776812] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.782762] Bluetooth: HIDP socket layer initialized
[ 1.789136] 8021q: 802.1Q VLAN Support v1.8
[ 1.793394] lib80211: common routines for IEEE802.11 drivers
[ 1.799196] 9pnet: Installing 9P2000 support
[ 1.803630] Key type dns_resolver registered
[ 1.808439] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.809364] registered taskstats version 1
[ 1.820618] Loading compiled-in X.509 certificates
[ 1.826718] mmc0: new high speed SDXC card at address 0001
[ 1.833745] mmcblk0: mmc0:0001 SD 58.2 GiB
[ 1.840170] mmcblk0: p1 p2
[ 1.864615] regulator-usb1-vcc GPIO handle specifies active low - ignored
[ 2.138654] ldo5: Bringing 1800000uV into 2500000-2500000uV
[ 2.151258] i2c i2c-0: IMX I2C adapter registered
[ 2.156726] imx8mq-usb-phy 381f0040.usb-phy: supply vbus not found, using dummy regulator
[ 2.165354] imx8mq-usb-phy 382f0040.usb-phy: supply vbus not found, using dummy regulator
[ 2.177504] pps pps0: new PPS source ptp0
[ 2.188050] fec 30be0000.ethernet eth0: registered PHC device 0
[ 2.195467] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[ 2.200993] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 1
[ 2.208768] xhci-hcd xhci-hcd.4.auto: hcc params 0x0220fe6c hci version 0x110 quirks 0x0000000001010010
[ 2.218226] xhci-hcd xhci-hcd.4.auto: irq 203, io mem 0x38100000
[ 2.224413] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[ 2.229924] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 2
[ 2.237606] xhci-hcd xhci-hcd.4.auto: Host supports USB 3.0 SuperSpeed
[ 2.245758] hub 1-0:1.0: USB hub found
[ 2.249557] hub 1-0:1.0: 1 port detected
[ 2.253826] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 2.262396] hub 2-0:1.0: USB hub found
[ 2.266190] hub 2-0:1.0: 1 port detected
[ 2.271682] xhci-hcd xhci-hcd.5.auto: xHCI Host Controller
[ 2.277213] xhci-hcd xhci-hcd.5.auto: new USB bus registered, assigned bus number 3
[ 2.284987] xhci-hcd xhci-hcd.5.auto: hcc params 0x0220fe6c hci version 0x110 quirks 0x0000000001010010
[ 2.294447] xhci-hcd xhci-hcd.5.auto: irq 204, io mem 0x38200000
[ 2.300614] xhci-hcd xhci-hcd.5.auto: xHCI Host Controller
[ 2.306127] xhci-hcd xhci-hcd.5.auto: new USB bus registered, assigned bus number 4
[ 2.313811] xhci-hcd xhci-hcd.5.auto: Host supports USB 3.0 SuperSpeed
[ 2.321334] hub 3-0:1.0: USB hub found
[ 2.325142] hub 3-0:1.0: 1 port detected
[ 2.329375] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[ 2.338474] hub 4-0:1.0: USB hub found
[ 2.342264] hub 4-0:1.0: 1 port detected
[ 2.346763] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1
[ 2.358892] galcore: clk_get 2d core clock failed, disable 2d/vg!
[ 2.358969] sdhci-esdhc-imx 30b50000.mmc: allocated mmc-pwrseq
[ 2.365361] Galcore version 6.4.11.p1.608260
[ 2.404679] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.451670] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu3d on minor 0
[ 2.460342] mxc_hantro 38300000.vpu: supply vpu not found, using dummy regulator
[ 2.467867] failed to set hantro voltage: 1000 mV
[ 2.472911] hantrodec: module inserted. Major = 510
[ 2.481041] input: gpio_keys as /devices/platform/gpio_keys/input/input1
[ 2.492004] input: bd718xx-pwrkey as /devices/platform/soc@0/30800000.bus/30a20000.i2c/i2c-0/0-004b/gpio-keys.1.auto/input/input2
[ 2.504563] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.516136] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.522781] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.525539] ALSA device list:
[ 2.531458] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 2.534510] No soundcards found.
[ 2.566240] mmc1: new high speed SDIO card at address 0001
[ 2.633534] EXT4-fs (mmcblk0p2): recovery complete
[ 2.641026] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Quota mode: none.
[ 2.649627] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.657992] devtmpfs: mounted
[ 2.661835] Freeing unused kernel memory: 3328K
[ 2.666469] Run /sbin/init as init process
[ 3.123635] systemd[1]: System time before build time, advancing clock.
[ 3.219433] systemd[1]: systemd 251.8+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN )
[ 3.251235] systemd[1]: Detected architecture arm64.
[ 3.316607] systemd[1]: Hostname set to <maaxboard>.
[ 3.417303] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000080
[ 3.426125] Mem abort info:
[ 3.426131] ESR = 0x0000000096000004
������D���ą�ą��@�D�����E�+HH��3.435430] SET = 0, FnV = 0
[ 3.438485] EA = 0, S1PTW = 0
[ 3.441627] FSC = 0x04: level 0 translation fault
[ 3.446509] Data abort info:
[ 3.449392] ISV = 0, ISS = 0x00000004
[ 3.453231] CM = 0, WnR = 0
[ 3.456201] user pgtable: 4k pages, 48-bit VAs, pgdp=00000000811e3000
[ 3.462648] [0000000000000080] pgd=0000000000000000, p4d=0000000000000000
[ 3.469449] Internal error: Oops: 0000000096000004 [#1] PREEMPT SMP
[ 3.475729] Modules linked in:
[ 3.478790] CPU: 2 PID: 171 Comm: systemd-system- Not tainted 6.1.1+gd59104ae45c4 #1
[ 3.483069] systemd-sysv-generator[172]: SysV service '/etc/init.d/sshd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package t.
[ 3.486540] Hardware name: Avnet MaaXBoard (DT)
[ 3.486544] pstate: 600000c5 (nZCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 3.486550] pc : pick_next_task_fair+0x118/0x310
[ 3.526141] lr : pick_next_task_fair+0x118/0x310
[ 3.530772] sp : ffff80000ac6ba30
[ 3.534088] x29: ffff80000ac6ba30 x28: 0000000000000000 x27: ffff80000ac6bbb8
[ 3.541236] x26: 0000000000000004 x25: ffff800009d76b40 x24: ffff000040c96ce8
[ 3.548382] x23: ffff000040c96740 x22: ffff000040c96740 x21: ffff0000415f5000
[ 3.555530] x20: ffff00004139ce00 x19: ffff00007fb8dac0 x18: 0000000000000000
[ 3.562677] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[ 3.569822] x14: 000000000000029c x13: 000000000000029c x12: 0000000000000001
[ 3.576968] x11: 0000000000000000 x10: 0000000000000001 x9 : ffff00007fb8db40
[ 3.584112] x8 : 0000000000000000 x7 : 00000000fffffffe x6 : 0000000000000000
[ 3.591257] x5 : 0000000000000006 x4 : 00000000fffffffd x3 : 0000012700000127
[ 3.598402] x2 : ffff80000997e510 x1 : 0000000000000000 x0 : 0000000000000000
[ 3.605549] Call trace:
[ 3.607998] pick_next_task_fair+0x118/0x310
[ 3.612280] __schedule+0x13c/0x710
[ 3.615777] schedule+0x5c/0xd0
[ 3.618924] io_schedule+0x3c/0x60
[ 3.622331] folio_wait_bit_common+0x174/0x340
[ 3.626783] filemap_fault+0x4d8/0x8fc
[ 3.630538] __do_fault+0x3c/0x204
[ 3.633946] __handle_mm_fault+0x8ec/0x10dc
[ 3.638136] handle_mm_fault+0xec/0x270
[ 3.641978] do_page_fault+0x150/0x450
[ 3.645735] do_translation_fault+0x9c/0xb0
[ 3.649926] do_mem_abort+0x44/0x94
[ 3.653420] el0_ia+0x58/0xe4
[ 3.656395] el0t_64_sync_handler+0xc4/0x120
[ 3.660669] el0t_64_sync+0x18c/0x190
[ 3.664340] Code: d65f03c0 d2800001 aa1403e0 97ffd923 (f9404014)
[ 3.670439] ---[ end trace 0000000000000000 ]---
[ 3.675060] note: systemd-system-[171] exited with preempt_count 2

U-Boot SPL 2022.04-lf_v2022.04+g0dd7e59924d (Sep 26 2023 - 07:43:51 +0000)
power_bd71837_init
set buck8 to 1.2v for DDR4
DDRINFO: start DRAM init
DDRINFO: DRAM rate 2400MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1


U-Boot 2022.04-lf_v2022.04+g0dd7e59924d (Sep 26 2023 - 07:43:51 +0000)

CPU: i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)
CPU: Commercial temperature grade (0C to 95C) at 35C
Reset cause: POR
Model: Avnet MaaXBoard
DRAM: 2 GiB
Core: 56 devices, 18 uclasses, devicetree: separate
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial

BuildInfo:
- ATF fccc380

switch to partitions #0, OK
mmc0 is current device
flash target is MMC:0
Net:
Warning: ethernet@30be0000 (eth0) using random MAC address - f2:44:f9:95:62:be
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
858 bytes read in 1 ms (837.9 KiB/s)
32512512 bytes read in 1355 ms (22.9 MiB/s)
52629 bytes read in 4 ms (12.5 MiB/s)
Applying DT overlay => ext-gpio.dtbo
575 bytes read in 2 ms (280.3 KiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004301ffff
Remove /soc@0/bus@30800000/ethernet@30be0000:phy-reset-gpios

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 6.1.1+gd59104ae45c4 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 12.2.0, GNU ld (GNU Binutils) 2.39.0.20220819) #1 SMP PREEMPT Thu Sep 7 06:56:02 UTC 2023
[ 0.000000] Machine model: Avnet MaaXBoard
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000044000000, size 960 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbfbc1700-0xbfbc3fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s44520 r8192 d29208 u81920
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc0,115200 console=tty1 root=/dev/mmcblk0p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] Memory: 1041108K/2097152K available (19904K kernel code, 1606K rwdata, 6788K rodata, 3328K init, 645K bss, 73004K reserved, 983040K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 8.33MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns
[ 0.000000] sched_clock: 56 bits at 8MHz, resolution 120ns, wraps every 2199023255541ns
[ 0.000460] Console: colour dummy device 80x25
[ 0.000931] printk: console [tty1] enabled
[ 0.001010] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.66 BogoMIPS (lpj=33333)
[ 0.001037] pid_max: default: 32768 minimum: 301
[ 0.001112] LSM: Security Framework initializing
[ 0.001219] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.001248] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.002820] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.002843] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.002933] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.003122] rcu: Hierarchical SRCU implementation.
[ 0.003136] rcu: Max phase no-delay instances is 1000.
[ 0.004272] EFI services will not be available.
[ 0.004502] smp: Bringing up secondary CPUs ...
[ 0.004986] Detected VIPT I-cache on CPU1
[ 0.005069] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.005110] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.005628] Detected VIPT I-cache on CPU2
[ 0.005702] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.005725] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.006190] Detected VIPT I-cache on CPU3
[ 0.006264] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.006287] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.006349] smp: Brought up 1 node, 4 CPUs
[ 0.006439] SMP: Total of 4 processors activated.
[ 0.006453] CPU features: detected: 32-bit EL0 Support
[ 0.006464] CPU features: detected: 32-bit EL1 Support
[ 0.006477] CPU features: detected: CRC32 instructions
[ 0.006556] CPU: All CPU(s) started at EL2
[ 0.006585] alternatives: applying system-wide alternatives
[ 0.008640] devtmpfs: initialized
[ 0.016224] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.016288] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.046124] pinctrl core: initialized pinctrl subsystem
[ 0.048244] DMI not present or invalid.
[ 0.048943] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.050154] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.050416] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.050584] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.050680] audit: initializing netlink subsys (disabled)
[ 0.050842] audit: type=2000 audit(0.048:1): state=initialized audit_enabled=0 res=1
[ 0.051387] thermal_sys: Registered thermal governor 'step_wise'
[ 0.051392] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.051437] cpuidle: using governor menu
[ 0.051634] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.051727] ASID allocator initialised with 65536 entries
[ 0.052667] Serial: AMBA PL011 UART driver
[ 0.052744] imx mu driver is registered.
[ 0.052772] imx rpmsg driver is registered.
[ 0.059690] imx8mq-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.069699] KASLR disabled due to lack of seed
[ 0.090409] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.090431] HugeTLB: 16380 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.090447] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.090461] HugeTLB: 508 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.090476] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.090491] HugeTLB: 28 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.090505] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.090519] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.092320] ACPI: Interpreter disabled.
[ 0.092886] iommu: Default domain type: Translated
[ 0.092901] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.093254] SCSI subsystem initialized
[ 0.093631] usbcore: registered new interface driver usbfs
[ 0.093681] usbcore: registered new interface driver hub
[ 0.093718] usbcore: registered new device driver usb
[ 0.094566] mc: Linux media interface: v0.10
[ 0.094610] videodev: Linux video capture interface: v2.00
[ 0.094681] pps_core: LinuxPPS API ver. 1 registered
[ 0.094695] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.094722] PTP clock support registered
[ 0.094856] EDAC MC: Ver: 3.0.0
[ 0.095781] FPGA manager framework
[ 0.095875] Advanced Linux Sound Architecture Driver Initialized.
[ 0.096481] Bluetooth: Core ver 2.22
[ 0.096521] NET: Registered PF_BLUETOOTH protocol family
[ 0.096534] Bluetooth: HCI device and connection manager initialized
[ 0.096552] Bluetooth: HCI socket layer initialized
[ 0.096567] Bluetooth: L2CAP socket layer initialized
[ 0.096592] Bluetooth: SCO socket layer initialized
[ 0.096908] vgaarb: loaded
[ 0.097376] clocksource: Switched to clocksource arch_sys_counter
[ 0.097571] VFS: Disk quotas dquot_6.6.0
[ 0.097620] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.097805] pnp: PnP ACPI: disabled
[ 0.105179] NET: Registered PF_INET protocol family
[ 0.105387] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.107217] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.107259] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.107286] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.107432] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 0.107919] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.108025] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.108091] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.108247] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.108574] RPC: Registered named UNIX socket transport module.
[ 0.108590] RPC: Registered udp transport module.
[ 0.108602] RPC: Registered tcp transport module.
[ 0.108613] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.109491] PCI: CLS 0 bytes, default 64
[ 0.110162] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.110787] kvm [1]: IPA Size Limit: 40 bits
[ 0.112347] kvm [1]: vgic-v2@31020000
[ 0.112371] kvm [1]: GIC system register CPU interface enabled
[ 0.112469] kvm [1]: vgic interrupt IRQ9
[ 0.112573] kvm [1]: Hyp mode initialized successfully
[ 0.113761] Initialise system trusted keyrings
[ 0.113927] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.121048] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.121815] NFS: Registering the id_resolver key type
[ 0.121858] Key type id_resolver registered
[ 0.121871] Key type id_legacy registered
[ 0.121962] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.121979] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.122013] ntfs: driver 2.1.32 [Flags: R/W].
[ 0.122173] ntfs3: Max link count 4000
[ 0.122186] ntfs3: Enabled Linux POSIX ACLs support
[ 0.122196] ntfs3: Read-only LZX/Xpress compression included
[ 0.122297] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.122654] 9p: Installing v9fs 9p2000 file system support
[ 0.166181] Key type asymmetric registered
[ 0.166196] Asymmetric key parser 'x509' registered
[ 0.166254] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.166274] io scheduler mq-deadline registered
[ 0.166287] io scheduler kyber registered
[ 0.171470] EINJ: ACPI disabled.
[ 0.179210] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.179244] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.182650] mxs-dma 33000000.dma-apbh: initialized
[ 0.186945] SoC: i.MX8MQ revision 2.1
[ 0.187053] Config NOC for VPU and CPU
[ 0.187645] Bus freq driver module loaded
[ 0.193045] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.195181] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 18, base_baud = 1562500) is a IMX
[ 1.275020] printk: console [ttymxc0] enabled
[ 1.280011] 30a60000.serial: ttymxc3 at MMIO 0x30a60000 (irq = 19, base_baud = 5000000) is a IMX
[ 1.300890] loop: module loaded
[ 1.305062] of_reserved_mem_lookup() returned NULL
[ 1.310053] megasas: 07.719.03.00-rc1
[ 1.314981] imx ahci driver is registered.
[ 1.323866] tun: Universal TUN/TAP device driver, 1.6
[ 1.329645] thunder_xcv, ver 1.0
[ 1.332916] thunder_bgx, ver 1.0
[ 1.336198] nicpf, ver 1.0
[ 1.340598] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.347841] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.353215] hclge is initializing
[ 1.356554] e1000: Intel(R) PRO/1000 Network Driver
[ 1.361446] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.367245] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.372224] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.378207] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.383626] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.389244] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.395527] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.401597] sky2: driver version 1.30
[ 1.405765] usbcore: registered new interface driver r8152
[ 1.411526] VFIO - User Level meta-driver version: 0.3
[ 1.419363] usbcore: registered new interface driver uas
[ 1.424739] usbcore: registered new interface driver usb-storage
[ 1.430829] usbcore: registered new interface driver usbserial_generic
[ 1.437393] usbserial: USB Serial support registered for generic
[ 1.443451] usbcore: registered new interface driver ftdi_sio
[ 1.449233] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.456591] usbcore: registered new interface driver usb_serial_simple
[ 1.463153] usbserial: USB Serial support registered for carelink
[ 1.469280] usbserial: USB Serial support registered for zio
[ 1.474977] usbserial: USB Serial support registered for funsoft
[ 1.481017] usbserial: USB Serial support registered for flashloader
[ 1.487409] usbserial: USB Serial support registered for google
[ 1.493373] usbserial: USB Serial support registered for libtransistor
[ 1.499934] usbserial: USB Serial support registered for vivopay
[ 1.505973] usbserial: USB Serial support registered for moto_modem
[ 1.512273] usbserial: USB Serial support registered for motorola_tetra
[ 1.518920] usbserial: USB Serial support registered for nokia
[ 1.524788] usbserial: USB Serial support registered for novatel_gps
[ 1.531175] usbserial: USB Serial support registered for hp4x
[ 1.536953] usbserial: USB Serial support registered for suunto
[ 1.542910] usbserial: USB Serial support registered for siemens_mpi
[ 1.549310] usbcore: registered new interface driver usb_ehset_test
[ 1.557954] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 1.572323] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.578546] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 1.587709] i2c_dev: i2c /dev entries driver
[ 1.596143] Bluetooth: HCI UART driver ver 2.3
[ 1.600617] Bluetooth: HCI UART protocol H4 registered
[ 1.605775] Bluetooth: HCI UART protocol BCSP registered
[ 1.611123] Bluetooth: HCI UART protocol LL registered
[ 1.616279] Bluetooth: HCI UART protocol ATH3K registered
[ 1.621713] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.628082] Bluetooth: HCI UART protocol Broadcom registered
[ 1.633778] Bluetooth: HCI UART protocol QCA registered
[ 1.640428] sdhci: Secure Digital Host Controller Interface driver
[ 1.646636] sdhci: Copyright(c) Pierre Ossman
[ 1.651575] Synopsys Designware Multimedia Card Interface Driver
[ 1.658121] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.667022] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.673826] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.680845] usbcore: registered new interface driver usbhid
[ 1.686437] usbhid: USB HID core driver
[ 1.694344] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.698266] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 1.706131] NET: Registered PF_LLC protocol family
[ 1.714119] NET: Registered PF_INET6 protocol family
[ 1.722234] Segment Routing with IPv6
[ 1.725966] In-situ OAM (IOAM) with IPv6
[ 1.729963] NET: Registered PF_PACKET protocol family
[ 1.735061] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 1.749688] Bluetooth: RFCOMM TTY layer initialized
[ 1.754620] Bluetooth: RFCOMM socket layer initialized
[ 1.759809] Bluetooth: RFCOMM ver 1.11
[ 1.763602] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.768949] Bluetooth: BNEP filters: protocol multicast
[ 1.774222] Bluetooth: BNEP socket layer initialized
[ 1.779219] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.785180] Bluetooth: HIDP socket layer initialized
[ 1.791845] 8021q: 802.1Q VLAN Support v1.8
[ 1.796062] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.797099] lib80211: common routines for IEEE802.11 drivers
[ 1.809232] mmc0: new high speed SDXC card at address 0001
[ 1.811624] mmcblk0: mmc0:0001 SD 58.2 GiB
[ 1.819564] 9pnet: Installing 9P2000 support
[ 1.819994] mmcblk0: p1 p2
[ 1.823968] Key type dns_resolver registered
[ 1.832071] registered taskstats version 1
[ 1.836209] Loading compiled-in X.509 certificates
[ 1.875663] regulator-usb1-vcc GPIO handle specifies active low - ignored
[ 2.224230] ldo5: Bringing 1800000uV into 2500000-2500000uV
[ 2.261583] i2c i2c-0: IMX I2C adapter registered
[ 2.267047] imx8mq-usb-phy 381f0040.usb-phy: supply vbus not found, using dummy regulator
[ 2.275660] imx8mq-usb-phy 382f0040.usb-phy: supply vbus not found, using dummy regulator
[ 2.287855] pps pps0: new PPS source ptp0
[ 2.298404] fec 30be0000.ethernet eth0: registered PHC device 0
[ 2.305830] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[ 2.311356] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 1
[ 2.319131] xhci-hcd xhci-hcd.4.auto: hcc params 0x0220fe6c hci version 0x110 quirks 0x0000000001010010
[ 2.328585] xhci-hcd xhci-hcd.4.auto: irq 203, io mem 0x38100000
[ 2.334776] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[ 2.340288] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 2
[ 2.347970] xhci-hcd xhci-hcd.4.auto: Host supports USB 3.0 SuperSpeed
[ 2.355606] hub 1-0:1.0: USB hub found
[ 2.359403] hub 1-0:1.0: 1 port detected
[ 2.363663] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 2.372751] hub 2-0:1.0: USB hub found
[ 2.376545] hub 2-0:1.0: 1 port detected
[ 2.382069] xhci-hcd xhci-hcd.5.auto: xHCI Host Controller
[ 2.387603] xhci-hcd xhci-hcd.5.auto: new USB bus registered, assigned bus number 3
[ 2.395374] xhci-hcd xhci-hcd.5.auto: hcc params 0x0220fe6c hci version 0x110 quirks 0x0000000001010010
[ 2.404832] xhci-hcd xhci-hcd.5.auto: irq 204, io mem 0x38200000
[ 2.410998] xhci-hcd xhci-hcd.5.auto: xHCI Host Controller
[ 2.416511] xhci-hcd xhci-hcd.5.auto: new USB bus registered, assigned bus number 4
[ 2.424197] xhci-hcd xhci-hcd.5.auto: Host supports USB 3.0 SuperSpeed
[ 2.431760] hub 3-0:1.0: USB hub found
[ 2.435558] hub 3-0:1.0: 1 port detected
[ 2.439793] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[ 2.448884] hub 4-0:1.0: USB hub found
[ 2.452677] hub 4-0:1.0: 1 port detected
[ 2.457168] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1
[ 2.469642] sdhci-esdhc-imx 30b50000.mmc: allocated mmc-pwrseq
[ 2.469770] galcore: clk_get 2d core clock failed, disable 2d/vg!
[ 2.481974] Galcore version 6.4.11.p1.608260
[ 2.511272] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.559837] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu3d on minor 0
[ 2.568717] mxc_hantro 38300000.vpu: supply vpu not found, using dummy regulator
[ 2.576229] failed to set hantro voltage: 1000 mV
[ 2.581245] hantrodec: module inserted. Major = 510
[ 2.587873] input: gpio_keys as /devices/platform/gpio_keys/input/input1
[ 2.597965] input: bd718xx-pwrkey as /devices/platform/soc@0/30800000.bus/30a20000.i2c/i2c-0/0-004b/gpio-keys.1.auto/input/input2
[ 2.610577] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.622669] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.623279] mmc1: new high speed SDIO card at address 0001
[ 2.629308] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.634516] ALSA device list:
[ 2.634522] No soundcards found.
[ 2.649745] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 2.675997] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Quota mode: none.
[ 2.684648] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.691768] devtmpfs: mounted
[ 2.695543] Freeing unused kernel memory: 3328K
[ 2.700165] Run /sbin/init as init process
[ 3.130652] systemd[1]: System time before build time, advancing clock.
[ 3.223674] systemd[1]: systemd 251.8+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN )
[ 3.255489] systemd[1]: Detected architecture arm64.
[ 3.329313] systemd[1]: Hostname set to <maaxboard>.
[ 3.351398] systemd[1]: Initializing machine ID from random generator.
[ 3.509499] systemd-sysv-generator[174]: SysV service '/etc/init.d/sshd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package t.
[ 3.952264] systemd[1]: Queued start job for default target Multi-User System.
[ 4.010685] systemd[1]: Created slice Slice /system/getty.
[ 4.017953] systemd[1]: Created slice Slice /system/modprobe.
[ 4.025202] systemd[1]: Created slice Slice /system/serial-getty.
[ 4.032423] systemd[1]: Created slice User and Session Slice.
[ 4.038483] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 4.046686] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 4.054603] systemd[1]: Reached target Path Units.
[ 4.059550] systemd[1]: Reached target Remote File Systems.
[ 4.065306] systemd[1]: Reached target Slice Units.
[ 4.070362] systemd[1]: Reached target Swaps.
[ 4.111473] systemd[1]: Listening on RPCbind Server Activation Socket.
[ 4.118492] systemd[1]: Reached target RPC Port Mapper.
[ 4.124325] systemd[1]: Listening on Syslog Socket.
[ 4.129555] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ 4.136674] systemd[1]: Listening on Journal Audit Socket.
[ 4.142543] systemd[1]: Listening on Journal Socket (/dev/log).
[ 4.148906] systemd[1]: Listening on Journal Socket.
[ 4.154438] systemd[1]: Listening on Network Service Netlink Socket.
[ 4.161310] systemd[1]: Listening on udev Control Socket.
[ 4.167074] systemd[1]: Listening on udev Kernel Socket.
[ 4.172763] systemd[1]: Listening on User Database Manager Socket.
[ 4.209764] systemd[1]: Mounting Huge Pages File System...
[ 4.219426] systemd[1]: Mounting POSIX Message Queue File System...
[ 4.225838] Unable to handle kernel paging request at virtual address ffff8000422244f8
[ 4.233786] Mem abort info:
[ 4.233789] ESR = 0x0000000096000005
[ 4.233792] EC = 0x25: DABT (current EL), IL = 32 bits
[ 4.233797] SET = 0, FnV = 0
[ 4.233799] EA = 0, S1PTW = 0
[ 4.233801] FSC = 0x05: level 1 translation fault
[ 4.233804] Data abort info:
[ 4.233805] ISV = 0, ISS = 0x00000005
[ 4.233807] CM = 0, WnR = 0
[ 4.233810] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000041e2c000
[ 4.233814] [ffff8000422244f8] pgd=10000000bffff003, p4d=10000000bffff003, pud=0000000000000000
[ 4.233824] Internal error: Oops: 0000000096000005 [#1] PREEMPT SMP
[ 4.233829] Modules linked in:
[ 4.233834] CPU: 3 PID: 180 Comm: mount Not tainted 6.1.1+gd59104ae45c4 #1
[ 4.233840] Hardware name: Avnet MaaXBoard (DT)
[ 4.233844] pstate: 800000c5 (Nzcv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 4.233850] pc : __find_get_block+0x74/0x3fc
[ 4.233865] lr : __getblk_gfp+0x2c/0x3c4
[ 4.233872] sp : ffff80000ac7b7b0
[ 4.233874] x29: ffff80000ac7b7b0 x28: ffff00004191bb00 x27: ffff0000414e8800
[ 4.233883] x26: 0000000000000000 x25: 0000000000000000 x24: ffff00004210be80
[ 4.233890] x23: 0000000000000008 x22: ffff800009b31648 x21: 0000000000001000
[ 4.233898] x20: 000000000000c926 x19: ffff8000422244e0 x18: 0000000000000000
[ 4.233905] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000
[ 4.233913] x14: 0000000000000000 x13: ffff000040829026 x12: ffff80000ac7bbe4
[ 4.233921] x11: 0000000f643add5b x10: 0000000000000002 x9 : 0000000000000004
[ 4.233928] x8 : 0000000000001000 x7 : ffff80000ac7b7b0 x6 : ffff80007606e000
[ 4.233936] x5 : 000000000000001e x4 : ffff800009b316c0 x3 : 000000000000000f
[ 4.378206] x2 : ffff800009b316c0 x1 : 0000000000000000 x0 : 0000000000000060
[ 4.378216] Call trace:
[ 4.378218] __find_get_block+0x74/0x3fc
[ 4.378227] __getblk_gfp+0x2c/0x3c4
[ 4.378236] ext4_getblk+0xa4/0x310
[ 4.378244] ext4_bread_batch+0x64/0x1d4
[ 4.378251] __ext4_find_entry+0x15c/0x420
[ 4.378257] ext4_lookup+0xa0/0x250
[ 4.378263] __lookup_slow+0x88/0x150
[ 4.378270] walk_component+0xd8/0x190
[ 4.378275] path_lookupat+0x78/0x1a0
[ 4.378281] filename_lookup+0xac/0x1a4
[ 4.378288] vfs_statx+0x8c/0x19c
[ 4.378295] vfs_fstatat+0x60/0x90
[ 4.378301] __do_sys_newfstatat+0x58/0xa0
[ 4.378308] __arm64_sys_newfstatat+0x20/0x30
[ 4.378316] invoke_syscall+0x48/0x114
[ 4.378325] el0_svc_common.constprop.0+0x44/0xec
[ 4.378332] do_el0_svc+0x2c/0xd0
[ 4.378339] el0_svc+0x2c/0x84
[ 4.378349] el0t_64_sync_handler+0xf4/0x120
[ 4.378354] el0t_64_sync+0x18c/0x190
[ 4.378364] Code: aa0403e2 d538d086 f8666853 b4ffff33 (f9400e62)
[ 4.378368] ---[ end trace 0000000000000000 ]---
[ 4.498277] systemd[1]: Mounting Kernel Debug File System...
[ 4.504837] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[ 4.527410] systemd[1]: Mounting Temporary Directory /tmp...
[ 4.536903] systemd[1]: Starting Create List of Static Device Nodes...
[ 4.546934] systemd[1]: Starting Load Kernel Module configfs...
[ 4.556353] systemd[1]: Starting Load Kernel Module drm...
[ 4.565332] systemd[1]: Starting Load Kernel Module fuse...
[ 4.580006] systemd[1]: Starting RPC Bind...
[ 4.584720] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[ 4.597334] fuse: init (API version 7.37)
[ 4.603063] systemd[1]: Starting Journal Service...
[ 4.618112] systemd[1]: Starting Load Kernel Modules...
[ 4.626905] systemd[1]: Starting Generate network units from Kernel command line...
[ 4.638534] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 4.649026] systemd[1]: Starting Coldplug All udev Devices...
[ 4.660852] systemd[1]: dev-hugepages.mount: Mount process exited, code=killed, status=11/SEGV
[ 4.669609] systemd[1]: dev-hugepages.mount: Failed with result 'signal'.
[ 4.670084] EXT4-fs (mmcblk0p2): re-mounted. Quota mode: none.
[ 4.677407] systemd[1]: Failed to mount Huge Pages File System.
[ 4.690813] systemd[1]: Started RPC Bind.
[ 4.695572] systemd[1]: Mounted POSIX Message Queue File System.
[ 4.701956] systemd[1]: Mounted Kernel Debug File System.
[ 4.707928] systemd[1]: Mounted Temporary Directory /tmp.
[ 4.714625] systemd[1]: Finished Create List of Static Device Nodes.
[ 4.722056] systemd[1]: modprobe@configfs.service: Deactivated successfully.
[ 4.729859] systemd[1]: Finished Load Kernel Module configfs.
[ 4.730654] mlan: loading out-of-tree module taints kernel.
[ 4.742432] systemd[1]: modprobe@drm.service: Deactivated successfully.
[ 4.750070] systemd[1]: Finished Load Kernel Module drm.
[ 4.756624] systemd[1]: modprobe@fuse.service: Deactivated successfully.
[ 4.764373] systemd[1]: Finished Load Kernel Module fuse.
[ 4.770559] systemd[1]: Started Journal Service.
[ 4.852755] wlan: Loading MWLAN driver
[ 4.858676] wlan: Register to Bus Driver...
[ 4.863431] wlan: Register to Bus Driver Done
[ 4.868354] systemd-journald[189]: Received client request to flush runtime journal.
[ 4.871599] wlan: Driver loaded successfully
[ 4.906853] Unable to handle kernel paging request at virtual address 000000000008b6c0
[ 4.914827] Mem abort info:
[ 4.917646] ESR = 0x0000000096000004
[ 4.921412] EC = 0x25: DABT (current EL), IL = 32 bits
[ 4.926739] SET = 0, FnV = 0
[ 4.929804] EA = 0, S1PTW = 0
[ 4.932947] FSC = 0x04: level 0 translation fault
[ 4.937839] Data abort info:
[ 4.940721] ISV = 0, ISS = 0x00000004
[ 4.944568] CM = 0, WnR = 0
[ 4.947549] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081ce1000
[ 4.954005] [000000000008b6c0] pgd=0000000000000000, p4d=0000000000000000
[ 4.960816] Internal error: Oops: 0000000096000004 [#2] PREEMPT SMP
[ 4.967089] Modules linked in: moal(O) mlan(O) fuse
[ 4.971984] CPU: 2 PID: 207 Comm: (d-sysctl) Tainted: G D O 6.1.1+gd59104ae45c4 #1
[ 4.980778] Hardware name: Avnet MaaXBoard (DT)
[ 4.985311] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 4.992280] pc : elv_attempt_insert_merge+0xcc/0x10c
[ 4.997260] lr : elv_attempt_insert_merge+0xb0/0x10c
[ 5.002232] sp : ffff80000ac5b5e0
[ 5.005548] x29: ffff80000ac5b5e0 x28: 0000000000080700 x27: ffff000040e13488
[ 5.012697] x26: ffff0000407b8e00 x25: ffff000040e13440 x24: ffff000040dd0000
[ 5.019843] x23: 0000000000000000 x22: ffff8000093e4bb8 x21: ffff000040949800
[ 5.026990] x20: ffff80000ac5b758 x19: ffff80000ac5b6b8 x18: ffff000040dd01a0
[ 5.034136] x17: 0000000091722d65 x16: 00000000000004c7 x15: 0000000000000000
[ 5.041281] x14: 0000000000067544 x13: 0000000000000000 x12: 00000000ffff8004
[ 5.048427] x11: 0000000000000011 x10: fffffc000009c740 x9 : 0000000000000004
[ 5.055573] x8 : 0000000000000004 x7 : 000000000005b630 x6 : 0000000000000000
[ 5.062719] x5 : 0000000000403000 x4 : 0000000000000000 x3 : 000000000004001a
[ 5.069864] x2 : ffff000040e13440 x1 : 000000000008b630 x0 : 0000000000000000
[ 5.077011] Call trace:
[ 5.079460] elv_attempt_insert_merge+0xcc/0x10c
[ 5.084089] blk_mq_sched_try_insert_merge+0x44/0x74
[ 5.089061] dd_insert_requests+0x84/0x2a0
[ 5.093164] blk_mq_sched_insert_requests+0xa4/0x264
[ 5.098133] blk_mq_flush_plug_list+0xd0/0x23c
[ 5.102585] __blk_flush_plug+0xf0/0x140
[ 5.106515] blk_finish_plug+0x38/0xf0
[ 5.110271] read_pages+0x170/0x2f4
[ 5.113766] page_cache_ra_unbounded+0x158/0x1dc
[ 5.118388] page_cache_ra_order+0x90/0x340
[ 5.122576] ondemand_readahead+0x174/0x2e4
[ 5.126763] page_cache_sync_ra+0x94/0xac
[ 5.130777] filemap_get_pages+0xb0/0x6a0
[ 5.134793] filemap_read+0xc0/0x344
[ 5.138374] generic_file_read_iter+0x100/0x18c
[ 5.142911] ext4_file_read_iter+0x50/0x180
[ 5.147100] __kernel_read+0xcc/0x244
[ 5.150767] kernel_read+0x68/0xb0
[ 5.154173] bprm_execve+0x1bc/0x59c
[ 5.157756] do_execveat_common.isra.0+0x198/0x240
[ 5.162554] __arm64_sys_execve+0x40/0x54
[ 5.166571] invoke_syscall+0x48/0x114
[ 5.170328] el0_svc_common.constprop.0+0xcc/0xec
[ 5.175039] do_el0_svc+0x2c/0xd0
[ 5.178360] el0_svc+0x2c/0x84
[ 5.181423] el0t_64_sync_handler+0xf4/0x120
[ 5.185701] el0t_64_sync+0x18c/0x190
[ 5.189373] Code: b5fffdf4 a94153f3 2a1703e0 a9425bf5 (f9401bf7)
[ 5.195473] ---[ end trace 0000000000000000 ]---
[ 5.200147] note: (d-sysctl)[207] exited with preempt_count 1
[ 5.206469] ------------[ cut here ]------------
[ 5.211100] WARNING: CPU: 3 PID: 207 at kernel/exit.c:765 do_exit+0x794/0x8fc
[ 5.218253] Modules linked in: moal(O) mlan(O) fuse
[ 5.223150] CPU: 3 PID: 207 Comm: (d-sysctl) Tainted: G D O 6.1.1+gd59104ae45c4 #1
[ 5.231947] Hardware name: Avnet MaaXBoard (DT)
[ 5.236481] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 5.243450] pc : do_exit+0x794/0x8fc
[ 5.247035] lr : do_exit+0x5c/0x8fc
[ 5.250528] sp : ffff80000ac5b1d0
[ 5.253845] x29: ffff80000ac5b1d0 x28: ffff8000097ef1b0 x27: ffff8000097ef1b8
[ 5.260992] x26: 0000000000000001 x25: ffff80000ac5b312 x24: 0000000000000000
[ 5.268140] x23: 0000000000000000 x22: 000000000000000b x21: ffff000041502100
[ 5.275285] x20: ffff0000407c1200 x19: ffff0000410b8ec0 x18: 0000000000000000
[ 5.282431] x17: 000000040044ffff x16: 00500072b5503510 x15: 0000000000000000
[ 5.289577] x14: ffff000040140ec0 x13: ffff80007606e000 x12: 0000000034d4d91d
[ 5.296723] x11: 0000000000000001 x10: 0000000000000a40 x9 : ffff80000ac5b120
[ 5.303870] x8 : ffff0000410b9960 x7 : ffff0000413fe200 x6 : 000000000016e360
[ 5.311016] x5 : 00000000410fd030 x4 : 0000000000f0000f x3 : ffff00004110d6c8
[ 5.318161] x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffff80000ac5b830
[ 5.325307] Call trace:
[ 5.327756] do_exit+0x794/0x8fc
[ 5.330996] make_task_dead+0x5c/0x100
[ 5.334753] die+0x200/0x23c +-----------------------------+
[ 5.337644] die_kernel_fault+0x264/0x364 | |
[ 5.341669] __do_kernel_fault+0xfc/0x18c | Cannot open /dev/ttyUSB1! |
[ 5.345697] do_page_fault+0xa8/0x450 | |
[ 5.349369] do_translation_fault+0x9c/0xb0 +-----------------------------+
[ 5.349376] do_mem_abort+0x44/0x94
[ 5.349383] el1_abort+0x40/0x64
[ 5.349391] el1h_64_sync_handler+0xd8/0xe4
[ 5.349396] el1h_64_sync+0x64/0x68
[ 5.367964] elv_attempt_insert_merge+0xcc/0x10c
[ 5.367973] blk_mq_sched_try_insert_merge+0x44/0x74
[ 5.367979] dd_insert_requests+0x84/0x2a0
[ 5.381651] blk_mq_sched_insert_requests+0xa4/0x264
[ 5.381658] blk_mq_flush_plug_list+0xd0/0x23c
[ 5.381667] __blk_flush_plug+0xf0/0x140
[ 5.381675] blk_finish_plug+0x38/0xf0
[ 5.381683] read_pages+0x170/0x2f4
[ 5.381689] page_cache_ra_unbounded+0x158/0x1dc
[ 5.381695] page_cache_ra_order+0x90/0x340
[ 5.381701] ondemand_readahead+0x174/0x2e4
[ 5.381707] page_cache_sync_ra+0x94/0xac
[ 5.381713] filemap_get_pages+0xb0/0x6a0
[ 5.381721] filemap_read+0xc0/0x344
[ 5.381728] generic_file_read_iter+0x100/0x18c
[ 5.381736] ext4_file_read_iter+0x50/0x180
[ 5.381743] __kernel_read+0xcc/0x244
[ 5.381749] kernel_read+0x68/0xb0
[ 5.381754] bprm_execve+0x1bc/0x59c
[ 5.381762] do_execveat_common.isra.0+0x198/0x240
[ 5.381772] __arm64_sys_execve+0x40/0x54
[ 5.381780] invoke_syscall+0x48/0x114
[ 5.381788] el0_svc_common.constprop.0+0xcc/0xec
[ 5.381795] do_el0_svc+0x2c/0xd0
[ 5.381802] el0_svc+0x2c/0x84
[ 5.381811] el0t_64_sync_handler+0xf4/0x120
[ 5.381815] el0t_64_sync+0x18c/0x190
[ 5.381822] ---[ end trace 0000000000000000 ]---

  • Sign in to reply
  • Cancel
  • msaka
    msaka 11 months ago

    Hi,

    Please refer to chapter 3 in this document, it is possible that the SD card was not setup correctly.

    https://www.avnet.com/wcm/connect/f67500b9-ba5a-4e56-98d2-b449c7bbacd2/MaaXBoard-Linux-Development_Guide-V1.0-EN.pdf?MOD=AJPERES&CACHEID=ROOTWORKSPACE.Z18_NA5A1I41L0ICD0ABNDMDDG0000-f67500b9-ba5a-4e56-98d2-b449c7bbacd2-nubVrw3?MOD=AJPERES&CACHEID=ROOTWORKSPACE.Z18_NA5A1I41L0ICD0ABNDMDDG0000-f67500b9-ba5a-4e56-98d2-b449c7bbacd2-nubVrw3

    Regards,

    Max.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • moose_rivieh
    moose_rivieh 11 months ago in reply to msaka

    My question is regarding YOCTO and not standalone linux development. The correct guide to reference for yocto development is listed below. We followed this guide step by step as well as meta-maaxboard readme as they both refer to different branches (mickledore vs. langdale). Neither images booted successfully. 

    Yocto build spits out an already formatted image (i.e. .wic) so it cannot be an sdcard image format.

    Have you built a yotcto generated image and were able to boot it on your hardware? 


    www.avnet.com/.../MaaXBoard-Linux-Yocto-UserManual-V2.1.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gonewtinwind
    gonewtinwind 11 months ago

    https://github.com/Avnet/meta-maaxboard/tree/mickledore 

    maaxboard  mickledore  branch works well. I did it a few month ago and fix the optee issue (you can see issue that I posted), please  just following the readme just that page.

    I have  a lot experience with maaxboard and maaxboard-mini. I can share with you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gonewtinwind
    gonewtinwind 11 months ago in reply to moose_rivieh

    do not need to read  www.avnet.com/.../MaaXBoard-Linux-Yocto-UserManual-V2.1.pdf first

    just following the guide here for  mickledore  branch

    https://github.com/Avnet/meta-maaxboard/tree/mickledore 

    I paste here:

    Yocto Setup

    Host setup

    To get the Yocto Project expected behavior in a Linux Host Machine, and the recommended minimum Ubuntu version is 20.04 or later. An important consideration is the hard disk space required in the host machine. It is recommended that at least 250 GB is provided, which is enough to compile all backends together.

    A Yocto Project build requires that some packages be installed for the build that are documented under the Yocto Project. Go to Yocto Project Quick Start and check for the packages that must be installed for your build machine. Essential Yocto Project host packages are:

    $ sudo apt-get update && sudo apt-get install -y \
    wget git-core diffstat unzip texinfo gcc-multilib \
    build-essential chrpath socat cpio python python3 python3-pip python3-pexpect \
    xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
    pylint3 xterm rsync curl gawk zstd lz4 locales bash-completion

    Repo setup

    Repo is a tool built on top of Git that makes it easier to manage projects that contain multiple repositories, which do not need to be on the same server. Repo complements very well the layered nature of the Yocto Project, making it easier for users to add their own layers to the BSP.

    Install or update repo to the latest version.

    $ mkdir -p ~/bin
    $ curl storage.googleapis.com/.../repo > ~/bin/repo
    $ chmod a+x ~/bin/repo
    $ export PATH=~/bin:$PATH

    Make sure that Git is set up properly with the following commands:

    $ git config --global user.name "Your Name"
    $ git config --global user.email "Your Email"
    $ git config --list

    Yocto setup

    The following example shows how to download the i.MX Yocto Project Community BSP recipe layers. For this example, a directory called imx-yocto-bsp is created for the project. Any name can be used instead of this.

    $ mkdir -p ~/imx-yocto-bsp
    $ cd ~/imx-yocto-bsp
    $ repo init -u github.com/.../imx-manifest -b imx-linux-mickledore -m imx-6.1.22-2.0.0.xml
    $ repo sync

    When this process is completed, the source code is checked out into the directory imx-yocto-bsp/sources. Then we need use following commands to clone this project (meta-maaxboard) to imx-yocto-bsp/sources folder.

    $ cd sources/
    $ git clone github.com/.../meta-maaxboard.git -b mickledore meta-maaxboard

    Yocto Build

    Build configurations

    MaaXBoard provides a script, maaxboard-setup.sh, that simplifies the setup for MaaXBoard serial boards. To use the script, the name of the specific machine to be built for needs to be specified. The script will sets up a directory and the configuration files for the specified machine.

    The syntax for the maaxboard-setup.sh script is shown below:

    $ MACHINE=<machine name> source sources/meta-maaxboard/tools/maaxboard-setup.sh -b <build dir>
    (eg: 
    machine name is 

    maaxboard maaxboard-mini
    • MACHINE= is the machine name which points to the configuration file in conf/machine in meta-maaxboard. Which should be maaxboard , maaxboard-mini, maaxboard-nano or maaxboard-8ulp.
    • -b specifies the name of the build directory created by the maaxboard-setup.sh script.

    Take MaaXBoard board as example, we can use following command to setup the Yocto build environment.

    $ cd ~/imx-yocto-bsp
    $ MACHINE=maaxboard source sources/meta-maaxboard/tools/maaxboard-setup.sh -b maaxboard/build

    If a new terminal window is opened or the machine is rebooted after a build directory is set up, the setup environment script should be used to set up the environment variables and run a build again. The full maaxboard-setup.sh is not needed.

    $ cd ~/imx-yocto-bsp
    $ source sources/poky/oe-init-build-env maaxboard/build

    Build an image

    The Yocto Project build uses the bitbake command. For example, bitbake builds the named component. Each component build has multiple tasks, such as fetching, configuration, compilation, packaging, and deploying to the target rootfs.

    The bitbake image build gathers all the components required by the image and build in order of the dependency per task. The first build is the toolchain along with the tools required for the components to build. The following command is an example on how to build an image:

    $ bitbake avnet-image-full

    here to find image : build/tmp/deploy/images/maaxboard/avnet-image-chromium( or full)-maaxboard-*.rootfs.wic.(bz2 ) if you set to .bz2 in local.conf, default is  wic

    I played maaxboard for a few year, I can share experience with you