Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed  DMA kernel module creation issues
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 267 views
  • Users 0 members are here
Related

Microzed  DMA kernel module creation issues

ghalady
ghalady over 12 years ago

Hi,
  I am attempting to integrate a PL Memory (BRAM) to the Microzed and run a Linux DMA test on PS from DDR to BRAM and vice-versa.

Here is what I have had success so far:
  I followed the instructions on http://www.wiki.xilinx.com/Build+Device+Tree+Blob

I was successful in building the dtb for the new BSP (with the PL memory-map added) from the system.dts that the Xilinx SDK creates.
However, now I don't know how to proceed. Should I rebuild the Kernel? I guess not, as the whole intent with which I started out was to create a "Kernel Module" of the DMA linux driver and load just the kernel module and not re-build the image.
Would appreciate if I get inputs on how to either build the kernel image or kernel module with the .dtb that I have!

Thanks
Girish

  • Sign in to reply
  • Cancel
Parents
  • ghalady
    0 ghalady over 12 years ago

    Have solved this issue, the DMA Driver need not be built, it is built in the git-linux source tree.  Could get the bitstream integrated and build the FSBL + bitstream + uBoot to create "boot.bin" using SDK and also create Linux uImage and device-tree.dtb.

    Issue now is in getting the dmatest to work on linux prompt "zynq" prompt.

    Would appreciate any inputs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ghalady
    0 ghalady over 12 years ago

    Have solved this issue, the DMA Driver need not be built, it is built in the git-linux source tree.  Could get the bitstream integrated and build the FSBL + bitstream + uBoot to create "boot.bin" using SDK and also create Linux uImage and device-tree.dtb.

    Issue now is in getting the dmatest to work on linux prompt "zynq" prompt.

    Would appreciate any inputs