Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design user push button
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 582 views
  • Users 0 members are here
Related

user push button

e14 Contributor
e14 Contributor over 12 years ago

Hi,

So I just would like to know with the SW1 which is a USER GPIO button. In the documentation it says it is connected to B9 and when checking UG865, this pin is connected to the PS. Is their a way of simply using it to trigger something in the PL? Or is there another way of triggering something in the PL with the microZed?

Ludwig

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You probably need to 'customize' the Zynq processing block to enable the GM Master AXI GP0 Interface. Then adding the axi_gpio block should give you a 'run connection automation' option.

     

    image

     

    If you are going to connect anything to the MicroZed Programmable Logic (PL) you are going to need to connect the MicroZed MicroHeaders, probably with one of the MicroZed Carrier Cards. The MicroZed IOCC carrier card has both user switches and push buttons as well as user LEDs on board that you could connect directly to GPIO.  http://zedboard.org/product/microzed-io-carrier-card

     

    The MicroZed FMC carrier card has user push buttons and LEDs you could connect to as well: http://zedboard.org/product/microzed-io-carrier-card

     

    If you do want to use the switch connected to the PS GPIO you can take a look at section 3 of the Zynq Concept Tools and Techniques for the Zedboard for an example of how to do that: http://zedboard.org/design/1521/11

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You probably need to 'customize' the Zynq processing block to enable the GM Master AXI GP0 Interface. Then adding the axi_gpio block should give you a 'run connection automation' option.

     

    image

     

    If you are going to connect anything to the MicroZed Programmable Logic (PL) you are going to need to connect the MicroZed MicroHeaders, probably with one of the MicroZed Carrier Cards. The MicroZed IOCC carrier card has both user switches and push buttons as well as user LEDs on board that you could connect directly to GPIO.  http://zedboard.org/product/microzed-io-carrier-card

     

    The MicroZed FMC carrier card has user push buttons and LEDs you could connect to as well: http://zedboard.org/product/microzed-io-carrier-card

     

    If you do want to use the switch connected to the PS GPIO you can take a look at section 3 of the Zynq Concept Tools and Techniques for the Zedboard for an example of how to do that: http://zedboard.org/design/1521/11

     

    -Gary