Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design 3v3 on uZed carrier card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 427 views
  • Users 0 members are here
Related

3v3 on uZed carrier card

smvo555
smvo555 over 11 years ago

Hi all,

I'm working on a custom carrier card for the Microzed and have been examining the differences between the power circuitry of the IO, FMC, and breakout carrier cards.

After careful review I can't see the harm in removing the 3v3 regulator from the design to save on board space. I will instead use the 5V line to enable the first regulator in the sequence.

I noticed the breakout carrier card does not have a 3v3 regulator but I'd rather use the MAX15066 based on the IO and FMC card designs because they can provide more output current.

Can anyone confirm my assertion about removing the 3v3 regulator? As far as the Zynq is concerned I only need to power the PL ports (no XADC)

Thanks,

Sam

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    0 ctammann over 11 years ago

    Hey Sam,

    3.3V is used for the FMC connector, the PMOD connectors as well as the LEDs and some level translators.  3.3V does not provide power directly to the SOM so if your carrier board doesn't need it you can remove it.  Just be very careful that you don't tie any signals to the FPGA to the 5V rail (such as LEDs without using a transistor).

    Just be sure that whatever you power the PL with matches the I/O signaling voltage level of the components on your carrier.
    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ctammann
    0 ctammann over 11 years ago

    Hey Sam,

    3.3V is used for the FMC connector, the PMOD connectors as well as the LEDs and some level translators.  3.3V does not provide power directly to the SOM so if your carrier board doesn't need it you can remove it.  Just be very careful that you don't tie any signals to the FPGA to the 5V rail (such as LEDs without using a transistor).

    Just be sure that whatever you power the PL with matches the I/O signaling voltage level of the components on your carrier.
    Thanks
    Chris