Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design 3v3 on uZed carrier card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 427 views
  • Users 0 members are here
Related

3v3 on uZed carrier card

smvo555
smvo555 over 11 years ago

Hi all,

I'm working on a custom carrier card for the Microzed and have been examining the differences between the power circuitry of the IO, FMC, and breakout carrier cards.

After careful review I can't see the harm in removing the 3v3 regulator from the design to save on board space. I will instead use the 5V line to enable the first regulator in the sequence.

I noticed the breakout carrier card does not have a 3v3 regulator but I'd rather use the MAX15066 based on the IO and FMC card designs because they can provide more output current.

Can anyone confirm my assertion about removing the 3v3 regulator? As far as the Zynq is concerned I only need to power the PL ports (no XADC)

Thanks,

Sam

  • Sign in to reply
  • Cancel
Parents
  • smvo555
    0 smvo555 over 11 years ago

    Thanks Chris,

    Actually, since the regulators are supplying VCCO I don't think my concerns about needing over 1A are valid. Anyone know why the beefier MAX15066 are used on the FMC and IO carrier card vs the LMR10510 on the breakout carrier card? What I don't like is the stack height of the inductor used in the MAX15066 circuit in the schematics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • smvo555
    0 smvo555 over 11 years ago

    Thanks Chris,

    Actually, since the regulators are supplying VCCO I don't think my concerns about needing over 1A are valid. Anyone know why the beefier MAX15066 are used on the FMC and IO carrier card vs the LMR10510 on the breakout carrier card? What I don't like is the stack height of the inductor used in the MAX15066 circuit in the schematics.