Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design HDMI FlowThru App? In MicroZed Vision Getting Started
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 403 views
  • Users 0 members are here
Related

HDMI FlowThru App? In MicroZed Vision Getting Started

e14 Contributor
e14 Contributor over 11 years ago

Starting out-of-the box with the MicroZed Embedded Vision Carrier Card using the MicroZed 7020.

I've followed the EMBV Getting Started Guide v1.zip
http://microzed.org/product/microzed-embedded-vision-kits

I'm using SD image downloaded from
EMBV - HDMI Passthrough Reference Design, Vivado 2014.4


I've progressed to page 19, successfully initiating serial communication with the processor, seeing dmesg following processor reset using SW2.

However, on step 18 of the Getting Started Guide I do not see the terminal output display what's shown in Figure 16... "Embedded Vision Carrier Card HDMI Pass-Through"  I simply see a "zynq>" prompt.  I can browse through the PS's file system but cannot locate the application to launch via command line.

Does the out of the box system support Embedded Vision Carrier Card HDMI Pass-Through?

A temporary complication is the kit did not include an FPGA programmer so I cannot configure the PL portion of the design.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Do you have the MicroZed boot jumper setting set to SD Card mode per the diagram on page 17 of the Getting Started Guide?

     

    It sounds like you are booting up a different image, one that just runs Linux, either from QSPI Flash, or a different SD Card image. If the boot jumpers are set correctly check and make sure that you have prepared your SD Card by erasing all existing content and then copying the image that is bundled with the Getting Started Guide Archive to the SD Card that has been formatted as FAT32.

     

    The boot.bin image will include the PL portion of the design and the Blue 'Done' LED (D2) on the MicroZed illuminating indicates that the PL has been configured.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Gary, very nice.  The orientation of the MicroZed (and my aging eyes) made it appear the jumpers were shipped configured for SD Card boot.  Not the case.  It was set for QSPI.

    Thanks.  I have pass through HDMI now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Gary, very nice.  The orientation of the MicroZed (and my aging eyes) made it appear the jumpers were shipped configured for SD Card boot.  Not the case.  It was set for QSPI.

    Thanks.  I have pass through HDMI now.