Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed not powering up
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 362 subscribers
  • Views 887 views
  • Users 0 members are here
Related

Microzed not powering up

100bobdxcool
100bobdxcool over 10 years ago

I bought 10 of microzed AES-Z7MB-7Z010-C01-I-G modules. But none of these seem to have jumpers nor rst or usr buttons. I was using a lower cost microzed AES-Z7MB-7Z010-SOM-G before. But when I power these new AES-Z7MB-7Z010-C01-I-G boards via USB, the LED's on the board do not blink at all. And my PC doesn't recognize this USB device at all. I put in the jumpers (set to SD card position), put an SD card which is working fine on the AES-Z7MB-7Z010-SOM-G boards, connected the  board to my PCB using the 100 pin connectors on the PCb and powered it. Still nothing happens. The LED's on the board dont blink at all. Can anyone please help em with this ?

AES-Z7MB-7Z010-SOM-G was working fine when connected to my PCB.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    Is your Carrier providing 5V through the MicroHeaders? Once the MicroZed is plugged into a Carrier, it is not intended for the system to be powered off the microUSB since the current limit is only 500mA for USB 2.0. We encourage designers to develop their own Carriers. We have a MicroZed Carrier Design Guide which should be useful for this purpose -- http://zedboard.org/support/documentation/1519.

     

    The board included in the AES-Z7MB-7Z010-G MicroZed Eval Kit is identical to the board included in AES-Z7MB-7Z010-SOM-G.

     

     Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100bobdxcool
    0 100bobdxcool over 10 years ago in reply to bhfletcher

    Thank you. So, for AES-Z7MB-7Z010-C01-I-G, there are no LEds that light up when powered via the carrier card. The only way to know if it boots up is connecting a micro usb to usb cable to the usb port on the PC and login to the board via putty or any other serial communication software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100bobdxcool
    0 100bobdxcool over 10 years ago in reply to bhfletcher

    Thank you. So, for AES-Z7MB-7Z010-C01-I-G, there are no LEds that light up when powered via the carrier card. The only way to know if it boots up is connecting a micro usb to usb cable to the usb port on the PC and login to the board via putty or any other serial communication software.