Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design USB UART connection fails with MicroZed, using Xilinx SDk 2015.4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 682 views
  • Users 0 members are here
Related

USB UART connection fails with MicroZed, using Xilinx SDk 2015.4

e14 Contributor
e14 Contributor over 10 years ago

I am following the example on Introduction to Zynq Hardware

: Running the "Hello World " Application.   Everything works as expected with building the hardware and exporting to SDK.   I do all of the following as instructed in the document:

1. Set Jumper to Cascaded JTAG Mode

2. Connected a USB cable between a PC and the microUSB port on Zed

3. Connected a Xilinx JTAG Programming Cable to J3

4. Use Device Manager to determine the COM port for the USB-UART

Next...In the Project Explore Window I right click on hello_world and select Run as > Run Configurations.  Right click Xilinx C/C++ application(GDB) and click New.

Now...When I click RUN in the Run Configuration window (according to the tutorial) a  message should appear asking if I want to launch the application even though configuration of the FPGA is not done.  BUT instead I get the ERROR says that Connection to Board Failed.  It looks like all the connections and drivers are there.  I would really like to understand what is going on here.

Thank you every one.


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi

    I rebuilt the application by following the simple MicroZed design in Vivado 2015.4.  I get a new error message says that Could not find FPGA device on the board for connection 'Local'.  Please let me what is happening here.

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi

    I rebuilt the application by following the simple MicroZed design in Vivado 2015.4.  I get a new error message says that Could not find FPGA device on the board for connection 'Local'.  Please let me what is happening here.

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi Zhu,
    I'm no expert but my question is, what jtag programmer are you using to connect to it? it sounds like SDK is not seeing your jtag programmer.
    Best,
    Rob