Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design USB UART connection fails with MicroZed, using Xilinx SDk 2015.4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 682 views
  • Users 0 members are here
Related

USB UART connection fails with MicroZed, using Xilinx SDk 2015.4

e14 Contributor
e14 Contributor over 10 years ago

I am following the example on Introduction to Zynq Hardware

: Running the "Hello World " Application.   Everything works as expected with building the hardware and exporting to SDK.   I do all of the following as instructed in the document:

1. Set Jumper to Cascaded JTAG Mode

2. Connected a USB cable between a PC and the microUSB port on Zed

3. Connected a Xilinx JTAG Programming Cable to J3

4. Use Device Manager to determine the COM port for the USB-UART

Next...In the Project Explore Window I right click on hello_world and select Run as > Run Configurations.  Right click Xilinx C/C++ application(GDB) and click New.

Now...When I click RUN in the Run Configuration window (according to the tutorial) a  message should appear asking if I want to launch the application even though configuration of the FPGA is not done.  BUT instead I get the ERROR says that Connection to Board Failed.  It looks like all the connections and drivers are there.  I would really like to understand what is going on here.

Thank you every one.


  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    If you do not follow the steps precisely for SDK it is possible for you to lose link.  To correct this I will typically close and restart SDK.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    If you do not follow the steps precisely for SDK it is possible for you to lose link.  To correct this I will typically close and restart SDK.

    --Dan