Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed temperature readings
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 518 views
  • Users 0 members are here
Related

MicroZed temperature readings

100padudle
100padudle over 9 years ago

Hello Guys,

I am running a design that runs the PL pretty hard in the Zynq 7020 on a MicroZed board.  In order to support that I instantiated the AXI4-Lite XADC core so that the PS can read the temperature under software control.

As a positive control I also read the supply voltages.  Here is the output of those readings.

VCCint = 0x000052B8, 0.969360 Volts
VCCaux = 0x0000999F, 1.800247 Volts
VCCbram = 0x000052FF, 0.972610 Volts
VCCpint = 0x00005480, 0.990234 Volts
VCCpaux = 0x000099C9, 1.802170 Volts
VCCoddr = 0x00007F1C, 1.489563 Volts
temperature = 0x0000B490, 82.314789 degrees C

All the power supply voltages look about right but the temperature measurement looks incorrect, 82C with the PL application not running.

I do not have a heatsink on the MicroZed and the ARM processors are just running Linux.  When I start the PL application the temperature rises to 104C.

What do you guys think?  Is 82C possible on a lightly loaded 7020?  What could I be doing to produce a wrong temperature reading?

I am using Equation 2-6 on page 33 of UG480 to compute degrees C from the register value and here is the C code that prints the temperature.

 read_val = read_reg(pcie_addr,XADC_TEMP);
    printf("temperature = 0x%08X, %f degrees C\n", read_val, ((0xffff&read_val)*503.975/(16.0*4096.0))-273.15);
 

 


 

  • Sign in to reply
  • Cancel
  • 100padudle
    0 100padudle over 9 years ago

    I should mention that the part feels hot but I can touch it. I would guess the case temperature is about 50 degrees C.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi padudle,

    Have you looked at the response to this forum post yet?

    http://zedboard.org/content/xadc-reference-design

    It should help you make sure everything is setup properly.

    --Josh