Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design boot from SDIO-1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 363 views
  • Users 0 members are here
Related

boot from SDIO-1

e14 Contributor
e14 Contributor over 12 years ago

Hello folks u2013

I posted this question on Xilinx website but have not heard anything so far - so I'm reaching out to the collective knowledge of Zedboard community for some guidance.

I developed a custom Zynq board (using Z-7020) that includes both QSPI Flash and SD memory. It is very similar to MicroZed - however due to the use of dual USBs - microSD card is attached to SDIO-1 port. I know from Zynq TRM that only SDIO-0 (not SDIO-1) could be used for first stage booting.

My question is have you guys managed to boot Linux image (image.ub for Petalinux) from SDIO-1 after loading the FSBL/bitstream/U-Boot from QSPI Flash?

In my case u2013 I managed to boot FSBL/Bitstream and U-Boot from QSPI Flash u2013 but when I do u201Crun sdbootu201D in U-Boot u2013 the system hangs up and never responds. I monitored the SDIO signals with a o-scope but there is nothing. Any feedback/guidance is appreciated.

Thanks.
Ted

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    Ted,

     

    We have not attempted to run secondary boot from SDIO-1. However, that should definitely be possible. Have you made any progress since this original post? Do you see any activity on the SDIO-1 lines at all?

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    >> My question is have you guys managed to boot Linux image (image.ub for Petalinux) from SDIO-1 after loading the FSBL/bitstream/U-Boot from QSPI Flash?

    Yes, I have. It's working fine.

    Do you have correctly configured the U-Boot? There is a definition in u-boot env that configure SD.

    u-boot-xlnx/include/configs/zynq_microzed.h

    In this file defined to use SD0: #define CONFIG_ZYNQ_SDHCI0
    You need tochange this define to: #define CONFIG_ZYNQ_SDHCI1

    and then "make zynq_microzed"