Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Problem using SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 362 subscribers
  • Views 1144 views
  • Users 0 members are here
Related

Problem using SD card

e14 Contributor
e14 Contributor over 11 years ago

Hi there,

I need some advice.  I am trying to use a SD card on a MicroZed board.  The board is loaded with a bare bones Zynq processor system all configured as per the board support package defaults.  I have booted linux on this board from that card before so know it is electrically all OK.  I am now just working on a basic SD card read and write using the Xilinx driver, no file system at this stage.  The code I am using is:

XSdPs_Config * sd0Cfg = XSdPs_LookupConfig(XPAR_PS7_SD_0_DEVICE_ID);//XPAR_PS7_SD_0_BASEADDR

int err = XSdPs_CfgInitialize(&sd0Inst, sd0Cfg, sd0Cfg->BaseAddress);

if(err == XST_SUCCESS)

{

err = XSdPs_SdCardInitialize(&sd0Inst);

if(err == XST_SUCCESS)

{

err = XSdPs_ReadPolled(&sd0Inst, 1, 1, buf);



}

}


The problem I have is that  XSdPs_SdCardInitialize fails UNLESS I step through it where it passes.  The problem happens somewhere in this code of  XSdPs_SdCardInitialize:

/*

* Send ACMD41 while card is still busy with power up

*/

while ((RespOCR & XSDPS_RESPOCR_READY) == 0) {

Status = XSdPs_CmdTransfer(InstancePtr, CMD55, 0, 0);

if (Status != XST_SUCCESS) {

Status = XST_FAILURE;

goto RETURN_PATH;

}



/*

* 0x40300000 - Host High Capacity support & 3.3V window

*/

Status = XSdPs_CmdTransfer(InstancePtr, ACMD41,

(XSDPS_ACMD41_HCS | XSDPS_ACMD41_3V3), 0);

if (Status != XST_SUCCESS) {

Status = XST_FAILURE;

goto RETURN_PATH;

}



/*

* Response with card capacity

*/

RespOCR = XSdPs_ReadReg(InstancePtr->Config.BaseAddress,

XSDPS_RESP0_OFFSET);



}

If I allow the processor to run to the first line of this code, then single step through it, then run again it succeeds!  It seems the only way it can fail is if one of the calls to XSdPs_CmdTransfer fails.  Not sure why they fail at full speed but OK on single stepping.

I have also tried changing the clock frequency to 25MHz and changing the pins slew rate to fast.  With the clock frequency the SD Init function seems to pass most times but the SD read function still fails every time.

Any advice would be greatly appreciated.  I will add any other information required if you ask.


Thanks

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi ashesman,

    Any reason why you need SD card access without using an operating system?

    It seems that others have come across similar challenges in getting this to work under baremetal execution.  Have you already reviewed these other forum threads?

    http://microzed.org/content/standalone-sd-card-sdio

    http://microzed.org/content/sd-card-example-design-using-standalone

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi ashesman,

    Any reason why you need SD card access without using an operating system?

    It seems that others have come across similar challenges in getting this to work under baremetal execution.  Have you already reviewed these other forum threads?

    http://microzed.org/content/standalone-sd-card-sdio

    http://microzed.org/content/sd-card-example-design-using-standalone

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Hi Kevin,

    Yes, I have read the threads.  There is one note in there about changing the SDIO and GPIO pins around which I did not quite understand.

    I am using an operating system, but not one that just works with this SDIO controller.  I am using FreeRTOS and its supported fat file system.  I will replace the ram disk implementation with SD card.  But, for now I can not even read a block from the card.  Once I can read and write to the card then I will use the OS.

    A little frustrating that the standard BSP and Vivado block automation do not just work to configure the SDIO and driver to just work.  I am sure it can be fixed...

    Cheers

    Ashley