Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed XADC pin documentation error?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 361 subscribers
  • Views 931 views
  • Users 0 members are here
Related

Microzed XADC pin documentation error?

e14 Contributor
e14 Contributor over 10 years ago

Hi,

The analog inputs share pins with LVDS inputs. So I wanted a pinout table with both ADC function and digital function. There isn't such a table that I found in the documentation, only separate tables for analog and digital (in the carrier design guide).

So I went a head and made one, and also double checked with the Xilinx package file. They do not match!

To me, it looks like table 5 in the carrier design guide is bad with 9 correct pairs and 7 bad (AD2,3,5,6,10,12,13).

For example, Xilinx puts AD3 together with IO_L9. L9 is called LVDS_8 by Microzed and is mapped to JX2_41,43 But Table five says AD3 is JX2_35,37

Anyone else seen this? Have I missed something?

References:
Carrier design guide: http://zedboard.org/sites/default/files/documentations/MicroZed_Carrier_Design_Guide_rev_1_5.pdf
Xilinx: http://www.xilinx.com/support/packagefiles/z7packages/xc7z020clg400pkg.txt

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Johan,

     

    I think you are being confused by the signal names used on the MicroZed JX connectors. It can happen easily as the board/ PCB signal names, such as JX2_LVDS_6P do NOT follow the same naming convention as the Xilinx Zynq signal names.

     

    JX2_LVDS_6P (which, as you mention above is connected to JX2-35) is in fact connected to the Zynq pin L19, which has a Xilinx signal name of IO_L9P_T1_DQS_AD3P_35. So it is XADC_AD3_P as shown in Table 5.

     

    I believe that the table is correct and you can verify by looking directly at the MicroZed schematic, which is available here:

     

    http://zedboard.org/support/documentation/1519

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thank you!

    You are right, I didn't check the numbering for all pins. When the first dozen was i numerical order I assumed the rest would be also, rather than being random. My fault.

    Do you know where I can find a table of the matching between pin names and Xilinx names and secondary functions? Feels a bit awkward to have to go back to the schematic for such basic things. Guess I'll just have to do one myself otherwise :-)

    Thanks for the help!

    Johan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Johan,

     

    Glad to help. We do have a table that cross references the MicroZed JX1 and JX2 signal names with the Zynq device signa names. It is the "MicroZed JX1 JX2 Pinout Tables" which can be found on the MicroZed documentaion page:

     

    http://zedboard.org/support/documentation/1519

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Those looks like what I need, except I get an error saying they reference an external file, and all the formula based names (the ones I need) just show an error. Is there a file missing, or (maybe more likely) is it because I open them with Open Office and not Excel?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Johan,

     

    I am able to open the file with the Excel viewer program. With the LibreOffice program I get a dialog about updating external files, but if I say 'no' I can open the file there as well. There are formulas embedded in the spreadsheet that reference an external file, a master constraints file, that I think were used to populate the spreadsheet automatically in the first place. 

     

    So the problem may be with Open Office. I would suggest either the Excel viewer if you are using windows or LibreOffice otherwise.

     

    -Gary