Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design SPI Self Test Fails
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 361 subscribers
  • Views 2749 views
  • Users 0 members are here
Related

SPI Self Test Fails

e14 Contributor
e14 Contributor over 11 years ago

I'm having trouble getting the SPI Self Test example to pass. I'm using Vivado 2014.4.


I checked both SPI peripherals in the "MIO Configuration" in Vivado. "ps7_spi_0" and "ps7_spi_1" both show up in system.mss in my BSP in the SDK. The base address for both peripherals is correct in "xparameters.h".


I imported the Xilinx example project "xspips_selftest_example" and ran it both for device ID 0 and 1 (SPI 0 and SPI 1) and both failed. The part it fails at is in the "int XSpiPs_SelfTest(XSpiPs *InstancePtr)" function it calls the "XSpiPs_Reset" function and then checks that the SPI registers are in their default state, which they are not which causes the test to fail.


Does anyone know where I can dig to find out why this test might be failing? Or maybe the test is out of date and shouldn't actually work in the first place? Thanks!


edit: To get into more detail of why the test is failing: The driver performs a reset on the SPI peripheral and then reads back the register value to see if it gets an expected value in the "Config_reg" register. The expected value is 0x00020000, but it actually reads back 0x00000000 which causes it to fail this test. I looked at the register value in Eclipse and it is indeed 0x00000000. I tried manually changing the register value and it has no effect, even though many of the bits are read/write according to the Technincal Reference Manual.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

    How to submit a case and send you the design file to investigate?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    This is the forum to post your questions. I would suggest starting a new forum thread as this is a new topic.

     

    Your description of the issue is confusing. You seem to be mixing the Zynq SPI controller and the AXI_QUAD_SPI controller. If you really are trying to use both I would suggest implementing and debugging one at a time. You mention PMOD J5 but there is not PMOD J5 on either the MicroZed or the MicroZed Embedded Vision Carrier Card.

     

    Please be specific on the boards you are using as well as the version of the Xilinx tools and your Host PC OS (Windows or Linux). You might also include a snippet of your xdc contraints file so that we can see how you have made your connections.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    This is the forum to post your questions. I would suggest starting a new forum thread as this is a new topic.

     

    Your description of the issue is confusing. You seem to be mixing the Zynq SPI controller and the AXI_QUAD_SPI controller. If you really are trying to use both I would suggest implementing and debugging one at a time. You mention PMOD J5 but there is not PMOD J5 on either the MicroZed or the MicroZed Embedded Vision Carrier Card.

     

    Please be specific on the boards you are using as well as the version of the Xilinx tools and your Host PC OS (Windows or Linux). You might also include a snippet of your xdc contraints file so that we can see how you have made your connections.

     

    -Gary